2024-05-07 04:35 AM
Hi,
I'm using stm32f103vet6 in my design, but due to the limit power budget, the MCU consumes much power(60mA per MCU , while I used 2 chips in my design), result in frequently triggering over current protection. Is there pin to pin compatible STM32L series part which could be utilized to replace the original one, so that I don't have to make hardware change?
Thanks.
Solved! Go to Solution.
2024-05-07 02:01 PM - edited 2024-05-07 02:02 PM
Dear @JKW , all,
My contribution to the thread - best replacement is STM32L4 series for both pin-to-pin compatibility with a 99% match to not say 100% ( due to the NC pin) just to wire to VDD - and will solve the power consumption as L4 series is on our best in class Cortex-M4 at 80MHz ULP line .
here LQFP100 column matters to migrate from F1 to L4.
Ciao
STOne-32
2024-05-07 04:43 AM
Doesn't CubeMX have a method of showing pin compatibility?
2024-05-07 04:55 AM
Hello,
You can use CubeMx tool / and cross Selector menu for that purpose:
For more details, refer to that knowledge base: https://community.st.com/t5/stm32-mcus/how-to-find-compatible-devices-for-an-mcu-stm32g473cb-as-example/ta-p/49636
2024-05-07 04:58 AM
It's quite helpful. Thanks a lot.
Further question, how can I evaluate the MCU power consumption if I change the STM32F to STM32L?
thanks.
2024-05-07 05:01 AM
Thanks for the hit. I tried it in CubeMX, there are quite a few compatible part . But I still have question for below:
If I deselect the 3 options, there is none candidates.
2024-05-07 05:01 AM - edited 2024-05-07 05:02 AM
Watch that video on Youtube: https://www.youtube.com/watch?v=gxvkgkJjI5A
Or refer to MCUs respective datasheets.
2024-05-07 11:46 AM
Pin-for-Pin compatibility is a battle ST's frequently lost.
The 144-pin device tending to be the least problematic.
The F1 series is very old, it's the first STM32 family, and ST learned some things. So there's usually now VCAP pins for the LDO, and some movement in the VDD/VSS pins, and a lot more flexibility in the peripheral pin mux/escape method. So there might be smaller parts that can get the functionality you need. Would look at G0 and C0 offerings.
The L series expect to be battery powered, all the time, and suspended, so they lack a different/separate VBAT pin
My expectation is that you'll have to spin the board, but changes might only need to be localized to the MCU and rearranging a handful of pins.
2024-05-07 02:01 PM - edited 2024-05-07 02:02 PM
Dear @JKW , all,
My contribution to the thread - best replacement is STM32L4 series for both pin-to-pin compatibility with a 99% match to not say 100% ( due to the NC pin) just to wire to VDD - and will solve the power consumption as L4 series is on our best in class Cortex-M4 at 80MHz ULP line .
here LQFP100 column matters to migrate from F1 to L4.
Ciao
STOne-32
2024-05-07 10:28 PM
Dear STOne-32,
question for the PIN NO.73, because the board assembled MCU is already there, but it;s NC pin in STM32F1 while it is VDD pin in STM32L4. In my board the NC pin is a no connection design, so I replace the chip with STM32L4, will it work, missing a VDD power supply?
2024-05-08 01:36 AM - edited 2024-05-08 09:05 AM
You need to connect that VDD pin otherwise you may face some issues.