‎2023-04-20 3:06 AM - edited ‎2023-11-20 7:38 AM
I configure the ADC1 of the STM32H735 like bellow:
The ADC Clock = 20MHz
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
/* ADC1 init function */
void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_MultiModeTypeDef multimode = {0};
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.NbrOfDiscConversion = 1;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc1.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_8CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
sConfig.OffsetSignedSaturation = DISABLE;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
void HAL_ADC_MspInit(ADC_HandleTypeDef* adcHandle)
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(adcHandle->Instance==ADC1)
{
/* USER CODE BEGIN ADC1_MspInit 0 */
/* USER CODE END ADC1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC;
PeriphClkInitStruct.PLL3.PLL3M = 2;
PeriphClkInitStruct.PLL3.PLL3N = 40;
PeriphClkInitStruct.PLL3.PLL3P = 2;
PeriphClkInitStruct.PLL3.PLL3Q = 5;
PeriphClkInitStruct.PLL3.PLL3R = 25;
PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL3VCIRANGE_3;
PeriphClkInitStruct.PLL3.PLL3VCOSEL = RCC_PLL3VCOWIDE;
PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL3;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* ADC1 clock enable */
__HAL_RCC_ADC12_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**ADC1 GPIO Configuration
PA0_C ------> ADC1_INP0
*/
HAL_SYSCFG_AnalogSwitchConfig(SYSCFG_SWITCH_PA0, SYSCFG_SWITCH_PA0_OPEN);
/* ADC1 DMA Init */
/* ADC1 Init */
hdma_adc1.Instance = DMA1_Stream1;
hdma_adc1.Init.Request = DMA_REQUEST_ADC1;
hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_adc1.Init.Mode = DMA_CIRCULAR;
hdma_adc1.Init.Priority = DMA_PRIORITY_MEDIUM;
hdma_adc1.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(adcHandle,DMA_Handle,hdma_adc1);
/* USER CODE BEGIN ADC1_MspInit 1 */
/* USER CODE END ADC1_MspInit 1 */
}
}
The ADC1_DR register = 0xFFE (I put 3.3V in PA0_C pin) it is ok.
but in the buffer, the dma transfer only the first byte :
I did not understand why the DMA always transfers a Byte despite I made several configuration combinations.
Best Regards,
‎2023-04-20 3:27 AM
Please show us the buffer declaration and how you start DMA.
‎2023-04-20 3:34 AM
And you could try:
hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
‎2023-04-20 3:53 AM
extern ADC_HandleTypeDef hadc1;
ALIGN_32BYTES (static uint16_t aADCxConvertedData[4]);
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
static void CPU_CACHE_Enable(void);
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_DMA_Init();
/* USER CODE BEGIN 2 */
HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
HAL_ADC_Start_DMA(&hadc1,(uint32_t*)aADCxConvertedData, 4 );
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
‎2023-04-20 3:55 AM
Same problem
‎2023-04-20 4:00 AM
Looks exactly like my working H7 ADC code.
‎2023-04-20 4:11 AM
I'm using ADC3 on a H723 / H735.
I don't see any GPIO init, is that included in HAL_SYSCFG_AnalogSwitchConfig() ?
There's this line in my init concerning ADC data alignment in the data register:
hAdc3.Init.DataAlign = ADC3_DATAALIGN_RIGHT;
Here's my working HAL setup, but I use multiple channels.
uint8_t ADC3_InitStartDma(void)
{
/* Configure the global features of the ADC:
* Clock, Resolution, Data Alignment and number of conversion
*/
hAdc3.Instance = ADC3;
hAdc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV32;
hAdc3.Init.Resolution = ADC_RESOLUTION_12B;
hAdc3.Init.DataAlign = ADC3_DATAALIGN_RIGHT;
hAdc3.Init.ScanConvMode = ADC_SCAN_ENABLE;
hAdc3.Init.ContinuousConvMode = ENABLE;
hAdc3.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hAdc3.Init.LowPowerAutoWait = DISABLE;
hAdc3.Init.NbrOfConversion = ADC_CHNL_MAX;
hAdc3.Init.DiscontinuousConvMode = DISABLE;
hAdc3.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hAdc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hAdc3.Init.DMAContinuousRequests = ENABLE;
hAdc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
hAdc3.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL;
hAdc3.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
//hAdc3.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hAdc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hAdc3.Init.OversamplingMode = DISABLE;
if( HAL_ADC_Init(&hAdc3) != HAL_OK ) Error_Handler_FL(__FILE__, __LINE__);
/* self calibration */
if( HAL_ADCEx_Calibration_Start(&hAdc3, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED ) != HAL_OK ) Error_Handler_FL(__FILE__, __LINE__);
return HAL_ADC_Start_DMA(&hAdc3, (uint32_t *)u16Adc3DmaBuffer, ADC_DMA_BUF_SIZE);
}
‎2023-04-20 4:12 AM
Man, that's ugly source code with my tab settings, sorry... :grinning_face_with_sweat:
‎2023-04-20 6:40 AM
@Saif​ Have you enabled the DMA interrupts somewhere?
/* ADC DMA interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);
‎2023-04-21 12:23 AM