cancel
Showing results for 
Search instead for 
Did you mean: 

TFT 16bit connections

Hector_06
Associate III

Hello Everyone 

I want connect stm32F LCd controller to TFT lcd but 16 bit  because I have lack of pins . how should I connect the RGB pins of STM32 to RGB pins of the LCD ? 

In case I use the LTDC contrller in 16bits , Can I use the unused pins  RGB of the controller  for other  fucntions ? 

 

Thank you in advanced 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,


I want connect stm32F LCd controller


Which STM32 part number? 

Please review the tips on how to post a thread in this community: https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228.

 


how should I connect the RGB pins of STM32 to RGB pins of the LCD ?  

You can refer to that application note: https://www.st.com/resource/en/application_note/an4861-introduction-to-lcdtft-display-controller-ltdc-on-stm32-mcus-stmicroelectronics.pdf


In case I use the LTDC contrller in 16bits , Can I use the unused pins  RGB of the controller  for other fucntions ?


Yes.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
SofLit
ST Employee

Hello,


I want connect stm32F LCd controller


Which STM32 part number? 

Please review the tips on how to post a thread in this community: https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228.

 


how should I connect the RGB pins of STM32 to RGB pins of the LCD ?  

You can refer to that application note: https://www.st.com/resource/en/application_note/an4861-introduction-to-lcdtft-display-controller-ltdc-on-stm32-mcus-stmicroelectronics.pdf


In case I use the LTDC contrller in 16bits , Can I use the unused pins  RGB of the controller  for other fucntions ?


Yes.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello  

 

We use STM32F429, and STM32UF9 

 

Regards 

Sami 

Ok. edited the post then .. PS: There is no STM32UF9 part number.

As said review the application note AN4861.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you , 

Should I connect the floating pins of the LCD to ground ?  or leave them floating ? 

 

 

Regards 

What do you mean by "floating pins of the LCD"?? RGB pins? in that case why? You said:

"In case I use the LTDC contrller in 16bits , Can I use the unused pins  RGB of the controller  for other fucntions ? "

So I understood you will use LCD with less pins of what available on STM32.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello 

The TFT  lcd  is 24 bits RGB ; I will use 16 bit  only and I will connect the  MCU STM32 to LCD as you suggested  in  AN4861

But my question 

What about the unused   pins now in the lcd , I have 8 data pin of the lcd not used ,  should I leave them floating ? 

or connect them to ground? 

 

Thank you 

I think you need to connect them to the GND but you need to refer to the datasheet of the LCD.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.