cancel
Showing results for 
Search instead for 
Did you mean: 

Switching from FDCAN mode to UART mode

Naresh_
Associate III

Hi,

 i am using STM32H753z  i try to switching FDCAN GPIO is PD0, PD1  to UART tx and rx (same pins)
now i changed FDCAN to UART tx side  is fine but in Rx side  i face issue ( no data is receiving to receive buffer).

 

 

#define CAN_AFR 0x99 #define UART_AFR 0x88 #define CHANGING_PORT 0xFFFFFFFA void switch_UART_TO_CAN(void) { if(HAL_UART_DeInit(&huart4) != HAL_OK) { Error_Handler(); } GPIOD->AFR[0] = CAN_AFR; GPIOD->MODER=CHANGING_PORT; MX_FDCAN1_Init(&hfdcan1); } void switch_CAN_TO_UART(void) { if(HAL_FDCAN_DeInit(&hfdcan1)!= HAL_OK) { Error_Handler(); } GPIOD->MODER=CHANGING_PORT; GPIOD->AFR[0] = UART_AFR; HAL_UART_Init(&huart4); MX_UART4_Init(); }

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

It's a bad idea to share the same pins between UART and FDCAN. Externally, the HW is not the same: CAN transceiver + a RS232 driver or STlink virtual comport.

So need to separate the pins.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

9 REPLIES 9
mÆŽALLEm
ST Employee

Hello,

You share USART4 and FDCAN1 pins, this supposes that FDCAN1 is seeing USART HW on its pins where you are switching to it! which is not recommended. You need to have free pins for FDCAN.

Which board are you using? Could you please share your schematics?

Also you have two UART4 init call which I couldn't understand:

HAL_UART_Init(&huart4); MX_UART4_Init();

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Method 1: void switch_UART_TO_CAN(void) { if(HAL_UART_DeInit(&huart4) != HAL_OK) { Error_Handler(); } GPIOD->AFR[0] = CAN_AFR; GPIOD->MODER=CHANGING_PORT; MX_FDCAN1_Init(&hfdcan1); } // void switch_CAN_TO_UART(void) { if(HAL_FDCAN_DeInit(&hfdcan1)!= HAL_OK) { Error_Handler(); } GPIOD->MODER=CHANGING_PORT; GPIOD->AFR[0] = UART_AFR; MX_UART4_Init(); } Method 2: void Switch_CAN_to_UART(void) { // Deinitialize FDCAN if (HAL_FDCAN_DeInit(&hfdcan1) != HAL_OK) { Error_Handler(); } GPIO_InitTypeDef GPIO_InitStruct = {0}; GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PIN_1; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF8_UART4; HAL_GPIO_Init(GPIOD, &GPIO_InitStruct); // Initialize UART MX_UART4_Init(); } void Switch_UART_to_CAN(void) { // Deinitialize UART if (HAL_UART_DeInit(&huart4) != HAL_OK) { Error_Handler(); } GPIO_InitTypeDef GPIO_InitStruct = {0}; GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PIN_1; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1; HAL_GPIO_Init(GPIOD, &GPIO_InitStruct); // Initialize CAN MX_FDCAN1_Init(); }
View more

i am transfer is happened in UART4 but in receive side HAL_UART_Receive()   thought time out error, issue

  

It's a bad idea to share the same pins between UART and FDCAN. Externally, the HW is not the same: CAN transceiver + a RS232 driver or STlink virtual comport.

So need to separate the pins.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi SofL,
Thank you quick  response,
   actually  my requirement is work both FDCAN AND UART IN same pin but different  time based commend from GUI(application )  when  GUI start they select CAN or UART at one time only 

to meet this requirement, i am going in this way.

Naresh__1-1721813989993.png

 

 

 

As stated before it's a bad idea to share the pins even one peripheral is used at a time. The FDCAN transceiver will disturb UART and seemingly UART HW (RS232 driver, STLINK VCOM or whatever attached) will disturb the FDCAN communication.

So need to separate the pins and dedicate pins for each interface or use a MUX on these pins.

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi, 

Thank you so mech, for quick response,

i have only one way is pin mux , can you please help me UART receive APis send time out error .

Sorry, I didn't understand this statement:,

i have only one way is pin mux , can you please help me UART receive APis send time out error .


But I think it's another subject related to UART usage itself not the pins sharing between the two interfaces. In that case please open a new thread.

Thank you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
LCE
Principal II

It's a little bit sad that nobody explains why this is not working...

The probable cause is a problem not related to the STM32:

When connecting 2 low impedance / push-pull outputs, one output "shorts" the other one.

This might only work with open-drain / open-collector outputs.

 

I think there is no need for this statement:


@LCE wrote:

It's a little bit sad that nobody explains why this is not working...

 

It's not a probable cause but it's definitely not related to the STM32.


@LCE wrote:

The probable cause is a problem not related to the STM32:

When connecting 2 low impedance / push-pull outputs, one output "shorts" the other one.

This might only work with open-drain / open-collector outputs.

 

Moreover, even in the inverse case (no output shorts), there will be an issue with CAN_Tx & UART_Rx / CAN_Rx & UART_Tx  sharing the same pins because the external transceiver/driver will force its output at a level that will disturb the current peripheral not using the driver/transceiver.

Conclusion: in both cases it's a bad idea to share the pins as stated above. So need to MUX them by an external HW.

 

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.