cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L496xx ADC accuracy specification (Datasheet 11585 Rev 15 page 189). The errors specified with the unit "LSB", does that count for 12 bit resolution? E.g. maximum offset error is 2.5 LSB12?

S.Nygaard
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @S.Nygaard​,

Welcome to the Community :) and thanks for your feedback.

The ADC spec LSB corresponds to the 12bit mode.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

3 REPLIES 3
TDK
Guru

Yes, it is. They should have noted 12-bit conversions in the "Conditions" panel, but didn't.

If you feel a post has answered your question, please click "Accept as Solution".
Imen.D
ST Employee

Hello @S.Nygaard​,

Welcome to the Community :) and thanks for your feedback.

The ADC spec LSB corresponds to the 12bit mode.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
S.Nygaard
Associate II

Thanks for the clarification