cancel
Showing results for 
Search instead for 
Did you mean: 

The Support Level of STM32MAT-TARGET for STM32H7xx series

ÇSütu.1
Associate II

Hi everyone,

I'm facing a problem where I don't have the flexibility to configure every peripheral of STM32H742VIT6 from Simulink. For instance when I want to use a TIM block in Simulink, it does not allow me to do so. Furthermore, the support for FDCAN is not included in Simulink. What should I do for this situation? Any comment or help is welcomed.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

STM32-MAT/TARGET is NRND status (not recommended for new designs), so I wouldn't expect any updates. Probably need to work with its current functionality or find a new solution.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks for the answer. Yes, probably I will manually insert the required code for those who are not supported(TIMERS, CAN, etc.).