2025-03-04 2:29 AM
Hello, I'm working on a project based on NUCLEO-WB55.USBDongle.
According to Zigbee specification paragraph 3.6.1.2 referring to to the NLME-PERMIT-JOINING.request procedure:
When this procedure is initiated with the PermitDuration parameter set to a value between 0x01 and 0xfe, the NLME shall set the macAssociationPermit PIB attribute in the MAC sub-layer to TRUE. The NLME shall then start a timer to expire after the specified duration. On expiration of this timer, the NLME shall set the macAssociation-Permit PIB attribute in the MAC sub-layer to FALSE
When this procedure is initiated with the PermitDuration parameter set to 0xff, the NLME shall set the macAssociationPermit PIB attribute in the MAC sub-layer to TRUE for an unlimited amount of time, unless another NLME-PERMIT-JOINING.request primitive is issued.
I implemented the following code on coordinator to update the join permit:
struct ZbZdoPermitJoinReqT req;
memset(&req, 0, sizeof(req));
req.destAddr = ZB_NWK_ADDR_BCAST_ROUTERS;
req.tcSignificance = true;
req.duration = ZB_PERMIT_JOIN_DURATION;
enum ZbStatusCodeT status = ZbZdoPermitJoinReq(zigbee_app_info.zb ,&req, NULL, NULL);
if (status != ZB_STATUS_SUCCESS) {
USB_DBG_PRINT(LOG_LEVEL_CRIT, ">> NWK | error 0x%02x. Cannot update join permit.", status);
}Everything works fine if ZB_PERMIT_JOIN_DURATION = 0xfe, but when I try to use ZB_PERMIT_JOIN_DURATION = 0xff I get an error code 0x80, corresponding to ZB_ZDP_STATUS_INV_REQTYPE. Am I missing something? Is the duration = 0xff not supported by the zigbee stack?
Also, is there any relevant difference in calling this function with .destAddr = ZB_NWK_ADDR_BCAST_ROUTERS vs .destAddr = ZB_NWK_ADDR_BCAST_ALL?
Solved! Go to Solution.
2025-03-04 8:47 AM - edited 2025-03-04 8:48 AM
Hello @tcpctrnk,
The valid range of PermitDuration is [0x00 : 0xFE]
The value 0x00 indicate that permission is disabled, other value between 0x01 and 0xFE is the amount of time in second to allow the join.
The Permit duration value of 0xFF has been removed starting from Zigbee R21 version.
Kind regards,
Ouadi
2025-03-04 8:47 AM - edited 2025-03-04 8:48 AM
Hello @tcpctrnk,
The valid range of PermitDuration is [0x00 : 0xFE]
The value 0x00 indicate that permission is disabled, other value between 0x01 and 0xFE is the amount of time in second to allow the join.
The Permit duration value of 0xFF has been removed starting from Zigbee R21 version.
Kind regards,
Ouadi
2025-03-04 9:01 AM
Thank you for the support @Ouadi !