2022-09-09 02:36 AM
Hello,
I'm planning to use a STM32L476 to acquire approx 150 analog signals.
For some reasons, I have to periodically check the justness of the ADCs.
I read in the RM that it is possible to connect internally DAC to ADC but I can not figure out how to select on which ADC & ADC channel the DAC output is "routed" to.
Can someone point me to info related to this ?
thanks
Solved! Go to Solution.
2022-09-09 05:37 AM
Hi @VDaanen ,
Thank you for sharing your request .
In fact the answer is in the RM (0351), section 18.4.11 "Channel selection (SQRx, JSQRx")
It is mentioned that :
As indicated on the schemas that you can also find in the RM
Please find in attached the document .
Best regards,
A.MVE
2022-09-09 05:25 AM
Hello VDaanen
According STM32L47xx RM0351 Rev 9, chapter 18 ADC, page 509 and 510.
Non Bufferized DAC1 and DAC2 channels are internally connected in single-ended to
Here the link:
Regards.
Romain
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-09-09 05:37 AM
Hi @VDaanen ,
Thank you for sharing your request .
In fact the answer is in the RM (0351), section 18.4.11 "Channel selection (SQRx, JSQRx")
It is mentioned that :
As indicated on the schemas that you can also find in the RM
Please find in attached the document .
Best regards,
A.MVE
2022-09-16 08:18 AM
Hi @VDaanen ,
Please let me know if you need more support for my side .
Otherwise if I gave you the right answer, select my answer as the best so that will help the others members to find the thread.
Best regards,
A.MVE