2018-11-11 01:48 AM
These solder bridges are in fact by default OFF, as these signals would collide with the LCD (as text elsewhere in the same manual points out).
May I at this point ask again for a table with describing connection of all pins on the target STM32L476, as it is in the current 'F4 DISCO manual?
Thanks,
JW
2018-11-12 09:07 AM
Hi Jan,
The error in "Solder bridges" table as well as the request to add the table " STM32 pin description versus board functions" are reported internally (to be assessed and check what can be done).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-11-12 09:08 AM
Thanks, Amel.
Jan