cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L432KBU6TR SPI 16 bit mode issue

Pinglei
Associate II

STM32L432KBU6 L432 chip, spi3, 16bit mode, 20M baud rate, spi output sclk is 16 cycles when it is powered on again after working for a period of time. Sometimes 15 cycles, sometimes 17 cycles, sometimes 16 cycles are output again. This will help confirm the reason, See the following documents for specific applications, thanks a lot. 

 

2 REPLIES 2
Pinglei
Associate II

Pinglei_0-1742281869895.png

 

Hello @Pinglei ,

First, "STM32L432KBU6TR" as title doesn't mean anything. You need to put a title that gives a raw idea of the subject while keeping it as short as possible. I've edited it to be "STM32L432KBU6TR SPI 16 bit mode issue".

Second, the issue is not clear.

Please review the tips on posting.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.