cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7x3 max SPI123 and SPI45 kernel clock freq?

TwelveSquared
Senior

I can't seem to find it in the datasheet: what is the max allowed kernel clock frequency for SPI123 and SPI45?

1 ACCEPTED SOLUTION
3 REPLIES 3

Usually the Kernel Clock Distribution Overview in the RM not the DM/DS

On the H745/H747 to hand SPI123 200MHz SPI45 125 MHz

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TwelveSquared
Senior

Thank you! I went crazy looking for that. Now I see it, in table 59 of the RM, rev 7. Thanks