cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H750 Performance slows down after time

sqwerize
Associate III

Hi!
I have a problem with the canbus gateway project, I have a very good ring buffer that works without delays and transfers data between can1 and can2. All data copying is done through the main while loop where I check the buffers for can1 and can2 to see if there is anything to send and handle it. The project works great, but after 2-3 hours of driving, strange anomalies start to happen... There is a second delay in data transfer, when I press the reset button on the art-pi board, everything returns to normal and works properly for the next 2-3 hours. I thought it might be a buffer overflow problem which can hold 512 messages for each can. However, when I turn off the vehicle and after a minute there are no frames on the bus and I restart the vehicle, the delay is still there... So it's not the buffers' fault. Has anyone encountered such a problem?

13 REPLIES 13

I seriously doubt anyone's got an apples-to-apples case for your issue / failure.

If you can't understand what your own code is doing, it's not clear how uninvolved parties are going to know.

Instrument things so you can better understand what's happening internally, and query / probe current state. Perhaps the ability to dump buffer, or memory structures, and reset buffering.

If using dynamic memory look at fragmentation and resource leaking.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
STOne-32
ST Employee

Dear @sqwerize ,

 

Also check the Clocks used on your system , a long term jitter may affect CAN bus . If possible to share your setup - crystal , PLL etc.

Hope it helps.

STOne-32

sqwerize
Associate III

@STOne-32 @Tesla DeLorean 

Here is screens and my ringbuffer:

 

sqwerize_7-1720994642276.png

sqwerize_0-1720994371581.pngsqwerize_1-1720994392309.pngsqwerize_2-1720994409458.pngsqwerize_3-1720994429826.png

sqwerize_4-1720994584264.pngsqwerize_5-1720994601295.pngsqwerize_6-1720994617735.png

 

mƎALLEm
ST Employee

Hello,

You need also to check if there were some errors on CAN communication. So activate the error interrupts, check also  TEC and REC counters.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hey, I found a similar problem on another forum, so maybe it's not entirely a canbus problem... 

https://forum.arduino.cc/t/stm32-performance-slowing-down-over-time/1005525

To my knowledge, we didn't have a such kind of issues from our customers.

The link you provided, the guy is using STM32F103 which is completely different from yours (STM32H750): different architecture, different CAN cell: STM32F103 has bxCAN cell (classical CAN)  while H7 has FDCAN cell were you are using it in CAN-FD mode. This means, most probably it's not related to the CAN HAL driver nor to the CAN cell. But from your usage of it: software of HW.

You need to instrument your code and check the CAN errors. There is no solution off the shelf in this kind of situation.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

The count++ count-- method of determining capacity/usage is not thread safe

Instrument so you can check if head and tail diverge when count reports as zero.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

This is almost certainly irrelevant to your situation.

Focus on understanding your own system dynamics and cause, not symptom of being slow.

Toggle a pin at 1 KHz in Systick and observe if you can scope 500 KHz signal. If it does, disabuse yourself that "STM32 running slowly" and move on to what the real problem is. If it does slow look at causes like unserviced interrupt storm or other saturation issues.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

This is a great idea to check the problem!!! Today I will try to do the tests this way and will come back with the results!
I don't use FreeRTOS because I had a very big performance drop and problems with accessing a resource at the same time, mutexes and semaphores didn't do very well.
Therefore, the main loop calls the function to flip data between can interfaces. In addition, timers add additional frames at intervals.