cancel
Showing results for 
Search instead for 
Did you mean: 

RSSI drop between full and extended BLE stack

Tyler_gajewski
Associate II

We are experiencing an issue with poor RSSI values on our STM32WB55 based custom board. We are normally running the extended ble stack and with only 3 feet between the windows PC and the STM32WB55 board were at RSSI values around -85.  When I switch to the Full BLE Stack I'm getting -50 values, I can go out the office, down the hall about 20 feet before I get the -85 db range.

I loaded the BLE_peripheral_lite example onto my board to test out if I had poor configuration and im getting good numbers 25 ft away, the example project requires the full stack. So I wanted to test the full with my board and software, and when I loaded the full im getting much better numbers. Similar to the example project.

Is there something related to the extended vs full stack that could be causing this issue?  Could this be a configuration issue in my software?

My current software almost 1-1 mimics the BLE_Peripheral_lite example for initializing cpu2.

Im testing with the 1.20 Extended BLE stack and the 1.19.1 Full BLE Stack.  My board has the STM32WB55RGV chip on it. 

Last I wanted to check was the antenna on my board vs the Nucleo board, so I loaded the BLE_Peripheral_lite onto both and im seeing identical RSSI performance with the full stack.

Edit: Closing this since it may have just been a noisy environment

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Tyler_gajewski 

The RSSI value should not be affected by the Stack that you are using. So, as you said the Noisy environment could be the reason behind the problem of this RSSI variation.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @Tyler_gajewski 

The RSSI value should not be affected by the Stack that you are using. So, as you said the Noisy environment could be the reason behind the problem of this RSSI variation.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.