2024-09-03 06:36 PM - edited 2024-09-04 02:07 PM
(Update: Comment moved here from STM32H745: DS and RM disagree, which to believe?)
I've also verified that these errors still exist (though table/page numbers have changed) in latest docs ("DS12923 Rev 2 March 2023" and "RM0399 Rev 4 June 2023"). These were reported 4 years ago, ST stated it would be fixed in the next revision. The next DS revision came out 3 years later and this was not fixed.
(Update: There is also a separate documentation error reported in Ethernet send complete interrupt not triggered in stm32f7 , which has similarly languished.)
Having a sluggish process is one thing - this is just dysfunctional.
Could you please follow up?
2024-09-04 07:06 AM - edited 2024-09-04 07:07 AM
Hi @BarryWhit ,
I prefer to start new thread here as a continuity of both discussions:
I let @STea investigate & take required actions asap.
I also invite @yilmazkircicek to follow here.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-04 12:49 PM - edited 2024-09-04 02:08 PM
Thank you @Amel NASRI. Sorry, there's no easy way for us to know who the right ST person is to try and bring in.
2024-09-05 07:42 PM
Anything?
2024-09-06 01:27 AM
Hi @BarryWhit ,
Internal requests will be made to relevant teams, we will share numbers with you for internal tracking purpose.
We will ensure the follow-up to have the corrections done. As these corrections are related to documentation, that may take some time to have them public.
Thanks for your understanding.
_Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-06 02:26 AM
Hello @BarryWhit and @yilmazkircicek
Thank you for your constructive feedback. we have been actively reinvestigating these issues. And here is an update on the status:
- @yilmazkircicek issue on PC13 absence in DS is confirmed and it is tracked on ticket 190362 (for internal reference only) to trigger the update of DS
- @BarryWhit documentation issue discussed in Ethernet send complete interrupt not triggered in stm32f7
are currently tracked in ticket 190373 (for internal reference only) and we will cascade the changes once confirmed to all the impacted products (F4 ,F2 ,F1 series)
Regards
2024-09-06 06:20 PM
Thank you both. I hope the process will go more smoothly this time around.