Skip to main content
Mike Ciholas
Associate II
Feb 6, 2020 5:47 PM UTC
Solved

STM32H745: DS and RM disagree, which to believe?

STM32H745 datasheet says:

RTC_OUT can come out PB2 port. No other port is listed in the DS for RTC_OUT. See table 8, page 62. RTC_OUT also listed in table 10, page 90, and note for PC13, page 92.

STM32H745 reference manual says:

RTC_OUT can be directed to PC13 or PB2, with PB2 not being useful in standby/VBAT modes. See table 387, page 2081.

Okay, so which document is correct?

My instincts say the RM likely is correct, but building PCBs based on instinct will end up costing you someday, so I want the documents to be clear and consistent.

This topic has been closed for replies.
Mohamed Aymen HZAMI
ST Employee
Feb 21, 2020 9:13 AM UTC

Hello,

The reference manual is the right one.

Best Regards,

Mohamed Aymen.

10 replies

Mohamed Aymen HZAMI
ST Employee
Feb 19, 2020 8:19 AM UTC

Hello,

After verification, we confirm this issue and will be fixed in the next release.

Thanks and Best Regards,

Mohamed Aymen.

waclawek.jan
Super User
Feb 19, 2020 9:28 AM UTC

Hi @Mohamed Aymen HZAMI​  ,

Ok so which one is correct?

JW

Piranha
Principal III
Feb 19, 2020 10:57 AM UTC

You know the modern rules - be polite, which actually means politically correct. Brain? Not required... :)

Piranha
Principal III
Feb 19, 2020 10:55 AM UTC

Also RM0399 is missing page 583, which makes PDF page numbers wrong after that page.

Mohamed Aymen HZAMI
ST Employee
Feb 24, 2020 1:48 PM UTC

Hello,

I raised this internally for correction and will be fixed in the next release.

Thanks and Best Regards,

Mohamed Aymen.

yilmazkircicek
Associate III
Sep 3, 2024 8:49 PM UTC

Now 2024, DS for the STM32H745XIH6 is the same...

Amel NASRI
ST Technical Moderator
Sep 4, 2024 2:08 PM UTC
To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.