cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H745: DS and RM disagree, which to believe?

Mike Ciholas
Associate III

STM32H745 datasheet says:

RTC_OUT can come out PB2 port. No other port is listed in the DS for RTC_OUT. See table 8, page 62. RTC_OUT also listed in table 10, page 90, and note for PC13, page 92.

STM32H745 reference manual says:

RTC_OUT can be directed to PC13 or PB2, with PB2 not being useful in standby/VBAT modes. See table 387, page 2081.

Okay, so which document is correct?

My instincts say the RM likely is correct, but building PCBs based on instinct will end up costing you someday, so I want the documents to be clear and consistent.

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,

The reference manual is the right one.

Best Regards,

Mohamed Aymen.

View solution in original post

10 REPLIES 10
Mohamed Aymen HZAMI
ST Employee

Hello,

After verification, we confirm this issue and will be fixed in the next release.

Thanks and Best Regards,

Mohamed Aymen.

Hi @Mohamed Aymen HZAMI​  ,

Ok so which one is correct?

JW

Piranha
Chief II

Also RM0399 is missing page 583, which makes PDF page numbers wrong after that page.

You know the modern rules - be polite, which actually means politically correct. Brain? Not required... :)

ST Support has confirmed PC13 supports RTC_OUT. They indicate the datasheet will be revised to reflect this option.

Hello,

The reference manual is the right one.

Best Regards,

Mohamed Aymen.

Thanks, Mohamed Aymen.

Jan

Hello,

I raised this internally for correction and will be fixed in the next release.

Thanks and Best Regards,

Mohamed Aymen.

yilmazkircicek
Associate III

Now 2024, DS for the STM32H745XIH6 is the same...