2020-05-09 7:13 PM
My STM32H743 SPI interrupt handler is being repeatedly called even though the interrupt enable register (IER) is 0. I'm running in slave mode and probably doing something really wrong for this to happen.
Here are the register values:
Name Value Access
CR1 0x00000001 ReadWrite
IOLOCK 0 ReadWrite
TCRCI 0 ReadWrite
RCRCI 0 ReadWrite
CRC33_17 0 ReadWrite
SSI 0 ReadWrite
HDDIR 0 ReadWrite
CSUSP 0 ReadWrite
CSTART 0 ReadWrite
MASRX 0 ReadWrite
SPE 1 ReadWrite
CR2 0x00000003 ReadWrite
TSER 0x0000 ReadWrite
TSIZE 0x0003 ReadWrite
CFG1 0x2000040F ReadWrite
CFG2 0x05000000 ReadWrite
IER 0x00000000 ReadWrite
TSERFIE 0 ReadWrite
MODFIE 0 ReadWrite
TIFREIE 0 ReadWrite
CRCEIE 0 ReadWrite
OVRIE 0 ReadWrite
UDRIE 0 ReadWrite
TXTFIE 0 ReadWrite
EOTIE 0 ReadWrite
DPXPIE 0 ReadWrite
TXPIE 0 ReadWrite
RXPIE 0 ReadWrite
SR 0xFFF80002 ReadOnly
CTSIZE 0xFFF8 ReadOnly
RXWNE 0 ReadOnly
RXPLVL 0x0 ReadOnly
TXC 0 ReadOnly
SUSP 0 ReadOnly
TSERF 0 ReadOnly
MODF 0 ReadOnly
TIFRE 0 ReadOnly
CRCE 0 ReadOnly
OVR 0 ReadOnly
UDR 0 ReadOnly
TXTF 0 ReadOnly
EOT 0 ReadOnly
DXP 0 ReadOnly
TXP 1 ReadOnly
RXP 0 ReadOnly
2020-05-09 7:34 PM
Is your NVIC SPI interrupt enabled? Look at VECTACTIVE to see which interrupt is really active. Might be a vector table issue.
2020-05-09 11:44 PM
> SPI interrupt handler is being repeatedly called
How do you know?
Which interrupt handler? What's its name?
Do you use Cube/HAL?
JW
2020-05-10 12:05 AM
Check the interrupt vectors.
Find the interrupt address offset in the Interrupt and exception vectors section of the reference manual.
Read the value at the address offset counted from the beginning of the flash, i.e. the address offset of the SPI4 interrupt is 0x190, then examine the value at 0x08000190. This is the address of the interrupt handler function.
Now find the address (minus 1) in the .map file. Is it your interrupt handler or something else?
2020-05-10 4:47 PM
Thaks for all your answers.
I'm partially using HAL.
Vector table looks correct and VTOR is correct.
I'm running from flash and it works up until a point.
I'm working on what point that is, but is it possible to get a SPI interrupt if IER is 0? I assume by all your responses that the answer is no.
2020-05-10 10:05 PM
Generally no, but it depends on what exactly do you mean by "SPI interrupt".
Answer the questions we've given.
JW
2020-05-11 6:14 AM
Interrupt handler is SPI4_IRQHandler.
Constantly hitting breakpoint in the handler.
What is VECTACTIVE?
Did I miss any questions?
2020-05-11 6:24 AM
Found VECTACTIVE.
Name Value Access
CPUID 0x411FC271
ICSR 0x04C46864
NMIPENDSET 0
PENDSVSET 0
PENDSVCLR 0
PENDSTSET 1
PENDSTCLR 0
ISRPENDING 1
VECTPENDING 0x46
RETTOBASE 1
VECTACTIVE 0x64
VTOR 0x08040000
AIRCR 0xFA050300
SCR 0x00000000
CCR 0x00040200
SHPR1 0x00000000
SHPR2 0x00000000
SHPR3 0xF0F00000
SHCRS 0x00000000
CFSR_UFSR_BFSR_MMFSR 0x00000000
HFSR 0x00000000
MMFAR 0x00000000
BFAR 0x00000000
2020-05-11 7:31 AM
In my EXTI interrupt handler for handling chip select transitions I enable the TXP interrupt on CS low. If I skip or remove that the problem goes away.
I need to send a status word as the first word. Since it can be changed by another task I need to place it in the FIFO on CS low.
void EXTI4_IRQHandler(void)
{
__HAL_GPIO_EXTI_CLEAR_IT(HostSPISelect_Pin);
GPIO_PinState state = HAL_GPIO_ReadPin(HostSPISelect_GPIO_Port, HostSPISelect_Pin);
if (state == GPIO_PIN_RESET) // CS active
{
__HAL_SPI_CLEAR_TXTFFLAG(hspi);
(*(__IO SPIDataType *)&hspi->Instance->TXDR) = StatusHeader;
__HAL_SPI_CLEAR_UDRFLAG(hspi);
hspi->pTxBuffPtr = (uint8_t *)aTxBuffer;
hspi->TxXferCount = hspi->TxXferSize;
__HAL_SPI_ENABLE_IT(hspi, SPI_IT_TXP);
__HAL_SPI_DISABLE_IT(hspi, SPI_IT_RXP);
...
2020-05-11 2:35 PM
So, you enable an SPI interrupt and the SPI interrupts? Where's the problem then?
JW