cancel
Showing results for 
Search instead for 
Did you mean: 

UART3 and UART4 interrupts together

NKale
Associate II


Hi,

I am using UART3 and UART4 interrupts together in STM32G070RBT6TR processor and facing issues.
I have inserted my service routines as below.

/* USER CODE BEGIN USART3_4_IRQn 0 */
if((USART4->ISR & USART_ISR_TC_Msk) == USART_ISR_TC_Msk){

}

if((USART3->ISR & USART_ISR_TC_Msk) == USART_ISR_TC_Msk){

}
/* USER CODE END USART3_4_IRQn 0 */


It is possible that, both interrupts can occur any time. It may happen that, one interrupt (USART4) occur while other (USART3) is being served.
At the end of service routine both interrupts are getting cleared (with below functions created by CubeMX) and may miss the one which occur later.
HAL_UART_IRQHandler(&huart3);
HAL_UART_IRQHandler(&huart4);
Can you provide me some pointer how to handle this situation?
Thanks in advance.

BR
Narendra

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

You can either use the HAL callbacks as intended, or you can handle the flags yourself. Doing a mix is not possible, as you may miss flags as outlined in your post.

The HAL callbacks will denote which flag was observed so that you can handle them there. The TC flag will cause the RX or TX complete callback to be called. I would recommend handling the TC flag in those callbacks.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

You can either use the HAL callbacks as intended, or you can handle the flags yourself. Doing a mix is not possible, as you may miss flags as outlined in your post.

The HAL callbacks will denote which flag was observed so that you can handle them there. The TC flag will cause the RX or TX complete callback to be called. I would recommend handling the TC flag in those callbacks.

If you feel a post has answered your question, please click "Accept as Solution".