cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h735 FDCAN not working

sid1401w
Associate

/* USER CODE BEGIN Header */

/* USER CODE END Header */

 

#include "main.h"

FDCAN_HandleTypeDef hfdcan1;

 

/* USER CODE BEGIN PV */

/* USER CODE END PV */

 

/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_FDCAN1_Init(void);

 

/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */

FDCAN_TxHeaderTypeDef TxHeader;

FDCAN_RxHeaderTypeDef RxHeader;

uint8_t TxData[8]={1,2,3,4,5,6,7,8};

uint8_t RxData[8];

uint32_t PutIndex;

int main(void)

{

 

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

 

/* USER CODE BEGIN Init */

/* USER CODE END Init */

 

/* Configure the system clock */

SystemClock_Config();

 

/* USER CODE BEGIN SysInit */

/* USER CODE END SysInit */

 

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_FDCAN1_Init();

/* USER CODE BEGIN 2 */

HAL_FDCAN_Start(&hfdcan1);

TxHeader.IdType = FDCAN_STANDARD_ID;

TxHeader.Identifier = 0x321;

 

TxHeader.TxFrameType = FDCAN_DATA_FRAME;

TxHeader.DataLength = FDCAN_DLC_BYTES_8;

TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;

TxHeader.BitRateSwitch = FDCAN_BRS_OFF;

TxHeader.FDFormat = FDCAN_CLASSIC_CAN;

TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;

TxHeader.MessageMarker = 0;

void FDCAN_CopyMessageToRAM(hfdcan1, TxHeader, TxData, PutIndex);

// HAL_StatusTypeDef FDCAN_CalcultateRamBlockAddresses(FDCAN_HandleTypeDef *hfdcan);

/* USER CODE END 2 */

 

/* Infinite loop */

/* USER CODE BEGIN WHILE */

while(1){

HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1,&TxHeader, TxData);

 

 

 

// HAL_FDCAN_GetRxMessage(&hfdcan1, FDCAN_RX_FIFO0, &RxHeader, RxData);

//

// HAL_Delay(1000);

//

}

 

}

/* USER CODE END WHILE */

 

/* USER CODE BEGIN 3 */

 

/* USER CODE END 3 */

 

 

/**

* @brief System Clock Configuration

* @retval None

*/

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 

/** Supply configuration update enable

*/

HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);

 

/** Configure the main internal regulator output voltage

*/

__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

 

while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 

/** Initializes the RCC Oscillators according to the specified parameters

* in the RCC_OscInitTypeDef structure.

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;

RCC_OscInitStruct.HSICalibrationValue = 64;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

RCC_OscInitStruct.PLL.PLLM = 4;

RCC_OscInitStruct.PLL.PLLN = 12;

RCC_OscInitStruct.PLL.PLLP = 2;

RCC_OscInitStruct.PLL.PLLQ = 12;

RCC_OscInitStruct.PLL.PLLR = 2;

RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;

RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;

RCC_OscInitStruct.PLL.PLLFRACN = 0;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2

|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;

RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;

RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;

 

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)

{

Error_Handler();

}

}

 

/**

* @brief FDCAN1 Initialization Function

* @param None

* @retval None

*/

static void MX_FDCAN1_Init(void)

{

 

/* USER CODE BEGIN FDCAN1_Init 0 */

 

/* USER CODE END FDCAN1_Init 0 */

 

/* USER CODE BEGIN FDCAN1_Init 1 */

 

/* USER CODE END FDCAN1_Init 1 */

hfdcan1.Instance = FDCAN1;

hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;

hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;

hfdcan1.Init.AutoRetransmission = DISABLE;

hfdcan1.Init.TransmitPause = DISABLE;

hfdcan1.Init.ProtocolException = DISABLE;

hfdcan1.Init.NominalPrescaler = 8;

hfdcan1.Init.NominalSyncJumpWidth = 1;

hfdcan1.Init.NominalTimeSeg1 = 13;

hfdcan1.Init.NominalTimeSeg2 = 2;

hfdcan1.Init.DataPrescaler = 1;

hfdcan1.Init.DataSyncJumpWidth = 1;

hfdcan1.Init.DataTimeSeg1 = 1;

hfdcan1.Init.DataTimeSeg2 = 1;

hfdcan1.Init.MessageRAMOffset = 4;

hfdcan1.Init.StdFiltersNbr = 0;

hfdcan1.Init.ExtFiltersNbr = 0;

hfdcan1.Init.RxFifo0ElmtsNbr = 1;

hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;

hfdcan1.Init.RxFifo1ElmtsNbr = 0;

hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;

hfdcan1.Init.RxBuffersNbr = 0;

hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;

hfdcan1.Init.TxEventsNbr = 0;

hfdcan1.Init.TxBuffersNbr = 0;

hfdcan1.Init.TxFifoQueueElmtsNbr = 0;

hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;

hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;

if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN FDCAN1_Init 2 */

FDCAN_FilterTypeDef sFiltr;

sFiltr.IdType=FDCAN_STANDARD_ID;

sFiltr.FilterConfig=FDCAN_FILTER_TO_RXFIFO0 ;

sFiltr.FilterType=FDCAN_FILTER_MASK;

sFiltr.FilterID1=0x004;

sFiltr.FilterID2=0x007;

sFiltr.FilterIndex=0;

HAL_FDCAN_ConfigFilter(&hfdcan1,&sFiltr);

/* USER CODE END FDCAN1_Init 2 */

 

}

 

/**

* @brief GPIO Initialization Function

* @param None

* @retval None

*/

static void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_InitStruct = {0};

/* USER CODE BEGIN MX_GPIO_Init_1 */

/* USER CODE END MX_GPIO_Init_1 */

 

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOH_CLK_ENABLE();

__HAL_RCC_GPIOC_CLK_ENABLE();

 

/*Configure GPIO pin Output Level */

HAL_GPIO_WritePin(GPIOC, GPIO_PIN_2, GPIO_PIN_RESET);

 

/*Configure GPIO pin : PC2 */

GPIO_InitStruct.Pin = GPIO_PIN_2;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 

/* USER CODE BEGIN MX_GPIO_Init_2 */

/* USER CODE END MX_GPIO_Init_2 */

}

 

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

 

/**

* @brief This function is executed in case of error occurrence.

* @retval None

*/

void Error_Handler(void)

{

/* USER CODE BEGIN Error_Handler_Debug */

/* USER CODE END Error_Handler_Debug */

}

 

 

2 REPLIES 2
KDJEM.1
ST Employee

Hello @sid1401w and welcome to the community :),

Could you please give more details about the issue? Which STM32CubeMX version are you using? Did you get a hard fault? 

I advise you to take a look and to start with an available FDCAN example.

For displaying code, I recommend you to use the </> button.

I hope this help you!

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

SofLit
ST Employee

Hello @sid1401w ,

As said by @KDJEM.1 you need to provide more details about your issue.

Also you need to provide information about your HW, schematics if possible.

How are you establishing the CAN bus? did you use transceiver as you are using CAN in normal mode? did you connect a second node on the bus?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.