2023-08-23 3:25 AM
Solved! Go to Solution.
2023-08-25 8:04 AM
2023-08-23 3:37 AM
Hello @wjian.2 :
Could you please provide more details, which STM32 product you are using?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-23 3:55 AM - edited 2023-08-23 3:59 AM
2023-08-23 9:39 AM
Repeatedly reposting basically the same topic to multiple threads is not helpful, pick one and stick with it.
2023-08-23 12:53 PM
I have a Nucleo-H723ZG where I was using a CAN transceiver on the Zio connector. After failure to get the CAN bus communcation working. I started to troubleshoot and I found that the schematic did not label the CAN RX/TX correctly. It was off by one pin.
If it's possible, you might want to ohm out the D1 which I assume is on the Arduino connector to the uC pin to see if there is a direct connection?
2023-08-25 8:04 AM