2024-01-23 6:04 AM - last edited on 2024-01-25 3:49 AM by mƎALLEm
I use STM32H562 and/or STM32H503 (nucleo board). When try in loop only this line:
while (1)
{
GPIOB->ODR ^= GPIO_PIN_6;
}
The frequency on pin is only 12.5 mhz. I use external quartz 8mhz (and 24mhz on nucleo)
I config to 250mhz (with build-in CubeMX ) :
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLL1_SOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 2;
RCC_OscInitStruct.PLL.PLLN = 125;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1_VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1_VCORANGE_WIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
}
Why is output frequency is too low ?. In assembler are no more 5 lines. So must be arround 50mhz.
2024-01-25 3:39 AM
and you set speed for mco hi ?
2024-01-25 7:11 AM
Yes i have set " very high" speed. I see other interestig: if i choice source to MCO1 to be HSE or CSI , on MCO1 pin have a signal. And signal is exacly frequency according source , BUT if i choice PLL1QCLK - NOT SIGNAL.:
2024-01-25 7:43 AM
btw
set the pll1 fractional divider :0
2024-01-25 8:08 AM
I set it 0 or other value , no mater. Just check and you will see that if you select for source PLL1Q - not signal !! Just test it. I see you dont trust me. JUST TEST !
2024-01-25 8:20 AM - edited 2024-01-25 8:23 AM
Seems you dont believe me....
as i said: i tested this first, to proove , i set clk correct.
>>>
<<<
try same setting (100M -> mco/10) - otherwise i have no idea, why it shouldnt work on your H563.
2024-01-25 8:26 AM
Do you have a kit with quarz as source not external generator ?
2024-01-25 8:31 AM
Its just original H563-nucleo board ; (un-modified...)
clk (8MHz) coming from st-linkV3 -> HSE bypass setting.
2024-01-25 8:31 AM
"try same setting (100M -> mco/10) - otherwise i have no idea, why it shouldnt work on your H563." - I check on H503 and H562.
Which is you version of HAL?
2024-01-25 8:38 AM
again ??
IDE v 1.13.1
2024-01-25 8:41 AM - edited 2024-01-25 8:41 AM
+ check, what Cube puzzling together in SystemClk_config:
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_PLL1Q, RCC_MCODIV_10);
}