cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0x0 WWDG timeout formula

SFrig.1
Associate

Can you confirm that the formula on the RM0454 manual to calculate the wwdg timeout is wrong?

0693W00000UoQxxQAF.png 

Shouldn't the WDGTB[1:0] parameter be WDGTB[2:0]?

Thank you

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @SFrig.1​, to the community!

Thanks for the contribution!

Yes, this is a typo and should be read as WDGTB[2:0].

Best regards

/Peter

@Amel NASRI​ 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KDJEM.1
ST Employee

Hello @SFrig.1​ & @Peter BENSCH​,

Thank you for bringing this issue to our attention.

I reported this issue internally.

Internal ticket number: 137183 (This is an internal tracking number and is not accessible or usable by customers).

Thank you

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.