cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f429: reading 2.5V issue as soon as I connect the source to the ADC input

harry123
Senior

Hi 

I'm trying to read a 2.5V signal through internal adc as soon as I connect the signal to the gpio pin of stm there is shift(to positive side)in the signal and also generating the noise upon seeing through oscilloscope.

Also made ground connection.

2 REPLIES 2

What pin on what board?

Check the schematic to understand what might be on the pin

Perhaps use a opamp so as not to load the signal.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Pin PA4 

Using voltage divider to lower the voltage from 46V to 2.5V and giving the signal to Stm.