cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong echo from STM32F4 USB device

SteMMo
Senior

Hi all,

I'm developing a composite USB device on USB OTG port on a board based on STM32F429 chip.

The device has two interfaces: a custom device + a CDC device. I'm using USB_Device_Library code.

Windows host correctly shows 3 items: the composite device, the generic USB device with my custom label/name, a virtual serial port (COM8).

As test when I open the virtual port (by Putty) I see the three-linee welcome message and a prompt.

When I press a key on the terminal, the code is sent to the device by a BulkOut packet and the device, if the code is different from 0x0d, echoes the code by a BulkIn packet.

This is OK til I press the nine-th character on  the keyboard: as echo of this character I see garbage on the terminal.

Dumping the memory of the internal buffers I see that the device received the correct code and replied 1 byte with the correct code!

If I sniff the usb channel with WireShark I see a 7-bytes packet on BulkIn reply (!!).

My debug log shows that the register containing the number of chars to sent to the host (IN_EP_TSIZ) is 1 and the char written in the FIFO (in USB_WritePacket fn) is 0x39 '9':

 

 

RXFLVL OUT DATA_UPD
RXFLVL DATA_UPD EP buff: x200100c1 - count: 1
OEPINT
OEPINT XFRC ep1
[USBD_LL_DataOutStage]
[USBD_LL_DataOutStage] DataOut ep1 - idx=1
[terminal] echo '9'
[transmit] x20010128, len: 1
[USB_EPStartXfer] IN_EP_TSIZ x00080001
IEPINT
IEPINT TXFE
[USB_WritePacket] ep2 - len: 1
[USB_WritePacket] IN_EP_TSIZ x00080001
[USB_WritePacket] x39
IEPINT
IEPINT XFRC ep2
[USBD_LL_DataInStage] ep2
[USBD_CDC_DataIn] ep2 - id=1
[USBD_CDC_DataIn] endTx TxBuf: x20010128 - 39 -

 

 

 How it is possible that Wireshark and Windows terminal reveive a 7-bytes packet ??? (None of them are 0x39)

 

Thanks!

7 REPLIES 7
FBL
ST Employee

Hi @SteMMo 

The issue is likely linked to endpoint configuration or the way the USB stack in CDC class driver handles the transmission. Could you share your code to reproduce on my board Nucleo F439?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

Hello!

Which ep configuration/parameter/register I can check?

In my case I'm using the IN 0x2 to send a single byte.

I'm in the OTG_FS_IRQHandler -> HAL_PCD_IRQHandler() when the USB_OTG_DIEPINT_TXFE interrupt is received for EP2.

Here I enter in the PCD_WriteEmptyTxFifo(), setup the ep variable mambers and len (=1) to call the USB_WritePacket() [stm32f4xx_ll_usb.c)] fn.

Here the variables are ok; pSrc points the buffer containing the byte, len=1 and count32b=1.

The registry values in the moment I write in the FIFO register (USB_WritePacket(..) in are:

DIEPCTRL2: 0x80888040

DIEPTSIZ2: 0x00080001

On the host side (Windows and Wireshark) I see a BULK IN dev-to-host 0x82 packet of 7 bytes as DataLength.

The routines are the 'standard' SDK involving stm32f4xx_hal_pcd.c and stm32f4xx_ll_usb.c files.

Thanks!

Just for completeness:

  • I'm working on a composite device: the serial port device is one of the two exposed classes.
  • the first one is a custom device and it is working well
  • the EPOUT 0x01 (host to dev) is correct; when I open a serial terminal on host and press a key, I receive the correct byte on device, the problem seems to be on EPIN 0x82 (dev to host)
  • the replies of CONTROL packets are correct, so i guess EP0 is good

 

Starting EP configuration:

CUSTOM device = 0x81, 0x02
CDC device = CMD 0x83, 0x82, 0x01

As said, CUSTOM device is detected and works well.

 

So, I tried to change the EP numbers:
CUSTOM device = 0x83, 0x01
CDC device = CMD 0x82, 0x81, 0x02

With this configuration the serial port is working, the custom device is detected as USB device, but it is not communicating and no IRQ are fired.

 

Another test - just to switched the EP numbers:

  • CDC EPs: 0x81 + 0x01 + CMD: 0x83
  • CUSTOM EPs: 0x82 + 0x02

The serial port is working well.

The custom device is detected but when I run my application  no interrupts are fired on STM32 (????).

 

Other test - switched again the EP numbers:

  • CDC EPs: 0x82 + 0x02 + CMD: 0x83
  • CUSTOM EPs: 0x81 + 0x01

The serial port is working well.

The custom device is detected but when I run my application  no interrupts are fired but the Wireshark session shows that host sends BULK_IN followed by FUNCTION_ABORT_PIPE. The device replied with a BULK_IN cancelled + a ACK on ABORT_PIPE.

 

 

 

Maybe I found the cause: the problem was the sum of all the TxFifo areas that was greater than 1.25kb, as stated from the Reference manual.

Remains the dubt about the switching of the EPs numbers: the original x82+x01 and 0x83+0x82+0x01 are the only working combination.

 

FBL
ST Employee

Hi @SteMMo 

I suggest you this article to learn more about How to select suitable endpoints for your STM32 US... - STMicroelectronics Community

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL