cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F405RGT6 CAN Reception Problem

STUser34
Associate II

I have been trying to resolve the issue for receiving the CAN interrupt but not able to find the root cause.

Hardware is a custom board micro is STM32F405RGT6 i am using CAN1 for CAN communication with 500 Kbps.

Able to transmit message CAN message using polling method. I am transmitting CAN messages from Peak CAN tool but not able to hit the receive interrupt.

Few observations after reset, the DBF bit is set, will it be a problem?

1.

STUser34_0-1715707247933.png

2.I have the Tx interrupt enabled

STUser34_1-1715707347339.png

But the TMEIE bit is not set after calling the MX_NVIC_Init(void)

STUser34_3-1715707652000.png

Coming to the actual problem the FMPIE0 bit is set and i am sending the messages at 1sec interval 

STUser34_4-1715707732840.png

FMP0 is always 0. What is the problem?

 

int main(void)
{

  /* USER CODE BEGIN 1 */
	/* USER CODE BEGIN 1 */
		TxHeader.IDE = CAN_ID_STD;
		TxHeader.StdId = 0x7df;
		TxHeader.RTR = CAN_RTR_DATA;
		TxHeader.DLC = 8;

		TxData[0] = 8;
		TxData[1] = 2;
		TxData[2] = 1;
		TxData[3] = 0xd;
		TxData[4] = 0;
		TxData[5] = 0;
		TxData[6] = 0;
		TxData[7] = 0;
		TxData[0] = 8;

		TxData1[0] = 8;
		TxData1[1] = 2;
		TxData1[2] = 1;
		TxData1[3] = 0x11;
		TxData1[4] = 0;
		TxData1[5] = 0;
		TxData1[6] = 0;
		TxData1[7] = 0;

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_CAN1_Init();

  /* Initialize interrupts */
  MX_NVIC_Init();
  /* USER CODE BEGIN 2 */
  CanFilter();
  /*To activate receive notification */
  if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
   {
    Error_Handler();
   }


  if (HAL_CAN_Start(&hcan1) != HAL_OK)
   {
    Error_Handler();
   }


  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
   HAL_GPIO_WritePin(GPIOC,GPIO_PIN_0,GPIO_PIN_RESET);
   HAL_GPIO_WritePin(GPIOC,GPIO_PIN_3,GPIO_PIN_RESET);
   if(HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData, &TxMailbox) != HAL_OK)
   {
	 Error_Handler ();
   }
   HAL_Delay(1000);
   while(HAL_CAN_IsTxMessagePending(&hcan1, TxMailbox));

   if (HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData1, &TxMailbox) != HAL_OK)
   {
	Error_Handler ();
   }


    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the main internal regulator output voltage
  */
  __HAL_RCC_PWR_CLK_ENABLE();
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL.PLLM = 8;
  RCC_OscInitStruct.PLL.PLLN = 64;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = 4;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief NVIC Configuration.
  * @retval None
  */
static void MX_NVIC_Init(void)
{
  /* FLASH_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(FLASH_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(FLASH_IRQn);
  /* RCC_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(RCC_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(RCC_IRQn);
  /* CAN1_TX_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(CAN1_TX_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(CAN1_TX_IRQn);
  /* CAN1_RX0_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn);
  /* CAN1_RX1_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(CAN1_RX1_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(CAN1_RX1_IRQn);
}

/**
  * @brief CAN1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_CAN1_Init(void)
{

  /* USER CODE BEGIN CAN1_Init 0 */

  /* USER CODE END CAN1_Init 0 */

  /* USER CODE BEGIN CAN1_Init 1 */

  /* USER CODE END CAN1_Init 1 */
  hcan1.Instance = CAN1;
  hcan1.Init.Prescaler = 2;
  hcan1.Init.Mode = CAN_MODE_NORMAL;
  hcan1.Init.SyncJumpWidth = CAN_SJW_3TQ;
  hcan1.Init.TimeSeg1 = CAN_BS1_9TQ;
  hcan1.Init.TimeSeg2 = CAN_BS2_6TQ;
  hcan1.Init.TimeTriggeredMode = DISABLE;
  hcan1.Init.AutoBusOff = DISABLE;
  hcan1.Init.AutoWakeUp = DISABLE;
  hcan1.Init.AutoRetransmission = ENABLE;
  hcan1.Init.ReceiveFifoLocked = DISABLE;
  hcan1.Init.TransmitFifoPriority = DISABLE;
  if (HAL_CAN_Init(&hcan1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN CAN1_Init 2 */

  /* USER CODE END CAN1_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0|GPIO_PIN_3, GPIO_PIN_RESET);

  /*Configure GPIO pin : PC0 */
  GPIO_InitStruct.Pin = GPIO_PIN_0;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_PULLDOWN;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

  /*Configure GPIO pin : PC3 */
  GPIO_InitStruct.Pin = GPIO_PIN_3;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void CanFilter(void)
{
	CAN_FilterTypeDef canfilterconfig;

	  canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
	  canfilterconfig.FilterBank = 18;  // which filter bank to use from the assigned ones
	  canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;
	  canfilterconfig.FilterIdHigh = 0x446<<5;
	  canfilterconfig.FilterIdLow = 0;
	  canfilterconfig.FilterMaskIdHigh = 0x446<<5;
	  canfilterconfig.FilterMaskIdLow = 0x0000;
	  canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
	  canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;
	  canfilterconfig.SlaveStartFilterBank = 20;  // how many filters to assign to the CAN1 (master can)

	  if (HAL_CAN_ConfigFilter(&hcan1, &canfilterconfig) != HAL_OK)
	    {
	     Error_Handler();
	    }
}

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
  if(HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
  {
    Error_Handler();
  }

  if ((RxHeader.StdId == 0x103))
  {
	 // datacheck = 1;
  }
}
/* USER CODE END 4 */

 

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

The image is not clear please share another one on which we can at least read the references.

Also for your filter config set a "pass all messages" filter as the following:

 

canfilterconfig.FilterIdHigh = 0;
canfilterconfig.FilterIdLow = 0;
canfilterconfig.FilterMaskIdHigh = 0;
canfilterconfig.FilterMaskIdLow = 0;

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

9 REPLIES 9
STUser34
Associate II

The TMEIE bit is set if i use the function

 if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_TX_MAILBOX_EMPTY) != HAL_OK)
     {
      Error_Handler();
     }

 

still the problem of CAN Rx interrupt exists, the isr is not called. 

Karl Yamashita
Lead III

Since it's a custom board, show us the schematic on how the CAN transceiver connection to the F405.

Also have you tried loop back mode? 

If smoke escapes your device, put the smoke back in. It'll still work as a conversation piece. If you find my answers useful, click the Accept as Solution button so that way others can see the solution.
SofLit
ST Employee

Hello,

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

Please don't use HSI for CAN communication. Use HSE with an external crystal.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

 I have enabled the HSE but no luck, there is no receive interrupt triggered. 

 

int main(void)
{

  /* USER CODE BEGIN 1 */
	/* USER CODE BEGIN 1 */
		TxHeader.IDE = CAN_ID_STD;
		TxHeader.StdId = 0x700;
		TxHeader.RTR = CAN_RTR_DATA;
		TxHeader.DLC = 8;

		TxData[0] = 8;
		TxData[1] = 2;
		TxData[2] = 1;
		TxData[3] = 0xd;
		TxData[4] = 0;
		TxData[5] = 0;
		TxData[6] = 0;
		TxData[7] = 0;
		TxData[0] = 8;

		TxData1[0] = 8;
		TxData1[1] = 2;
		TxData1[2] = 1;
		TxData1[3] = 0x11;
		TxData1[4] = 0;
		TxData1[5] = 0;
		TxData1[6] = 0;
		TxData1[7] = 0;

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_CAN1_Init();

  /* Initialize interrupts */
  MX_NVIC_Init();
  /* USER CODE BEGIN 2 */
  CanFilter();
  /*To activate receive notification */
  if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
   {
    Error_Handler();
   }

   if (HAL_CAN_Start(&hcan1) != HAL_OK)
   {
    Error_Handler();
   }


  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
   HAL_GPIO_WritePin(GPIOC,GPIO_PIN_0,GPIO_PIN_RESET);
   HAL_GPIO_WritePin(GPIOC,GPIO_PIN_3,GPIO_PIN_RESET);
   if(HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData, &TxMailbox) != HAL_OK)
   {
	 Error_Handler ();
   }
   HAL_Delay(1000);
   while(HAL_CAN_IsTxMessagePending(&hcan1, TxMailbox));

   if (HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData1, &TxMailbox) != HAL_OK)
   {
	Error_Handler ();
   }


    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the main internal regulator output voltage
  */
  __HAL_RCC_PWR_CLK_ENABLE();
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 8;
  RCC_OscInitStruct.PLL.PLLN = 64;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = 4;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief NVIC Configuration.
  * @retval None
  */
static void MX_NVIC_Init(void)
{
  /* FLASH_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(FLASH_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(FLASH_IRQn);
  /* RCC_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(RCC_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(RCC_IRQn);
  /* CAN1_RX0_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn);
  /* CAN1_RX1_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(CAN1_RX1_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(CAN1_RX1_IRQn);
}

/**
  * @brief CAN1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_CAN1_Init(void)
{

  /* USER CODE BEGIN CAN1_Init 0 */

  /* USER CODE END CAN1_Init 0 */

  /* USER CODE BEGIN CAN1_Init 1 */

  /* USER CODE END CAN1_Init 1 */
  hcan1.Instance = CAN1;
  hcan1.Init.Prescaler = 2;
  hcan1.Init.Mode = CAN_MODE_NORMAL;
  hcan1.Init.SyncJumpWidth = CAN_SJW_3TQ;
  hcan1.Init.TimeSeg1 = CAN_BS1_9TQ;
  hcan1.Init.TimeSeg2 = CAN_BS2_6TQ;
  hcan1.Init.TimeTriggeredMode = DISABLE;
  hcan1.Init.AutoBusOff = DISABLE;
  hcan1.Init.AutoWakeUp = DISABLE;
  hcan1.Init.AutoRetransmission = ENABLE;
  hcan1.Init.ReceiveFifoLocked = DISABLE;
  hcan1.Init.TransmitFifoPriority = DISABLE;
  if (HAL_CAN_Init(&hcan1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN CAN1_Init 2 */

  /* USER CODE END CAN1_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0|GPIO_PIN_3, GPIO_PIN_RESET);

  /*Configure GPIO pin : PC0 */
  GPIO_InitStruct.Pin = GPIO_PIN_0;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_PULLDOWN;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

  /*Configure GPIO pin : PC3 */
  GPIO_InitStruct.Pin = GPIO_PIN_3;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void CanFilter(void)
{
	CAN_FilterTypeDef canfilterconfig;

	  canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
	  canfilterconfig.FilterBank = 18;  // which filter bank to use from the assigned ones
	  canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;
	  canfilterconfig.FilterIdHigh = 0x446<<5;
	  canfilterconfig.FilterIdLow = 0;
	  canfilterconfig.FilterMaskIdHigh = 0x446<<5;
	  canfilterconfig.FilterMaskIdLow = 0x0000;
	  canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
	  canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;
	  canfilterconfig.SlaveStartFilterBank = 20;  // how many filters to assign to the CAN1 (master can)

	  if (HAL_CAN_ConfigFilter(&hcan1, &canfilterconfig) != HAL_OK)
	    {
	     Error_Handler();
	    }
}

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
  if(HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
  {
    Error_Handler();
  }

  if ((RxHeader.StdId == 0x103))
  {
	 // datacheck = 1;
  }
}

I have not tried the loop back mode, i will try that as well. 

STUser34_0-1715735984476.png

I am not sure if the image is clear i will share the scanned image after some time.

The image is not clear please share another one on which we can at least read the references.

Also for your filter config set a "pass all messages" filter as the following:

 

canfilterconfig.FilterIdHigh = 0;
canfilterconfig.FilterIdLow = 0;
canfilterconfig.FilterMaskIdHigh = 0;
canfilterconfig.FilterMaskIdLow = 0;

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you so much it worked now. 

You didn't show how the F407 is connected so don't know where the RS line of the transceiver is connected to? But i am going to take a guess that PORTC pin 1 or pin 3 controls the RS line? 

Have you checked the TP13 with an oscilloscope to see if you're getting a CAN message? Maybe check the air core to be sure signals are on both High and low side to the transceiver.

If smoke escapes your device, put the smoke back in. It'll still work as a conversation piece. If you find my answers useful, click the Accept as Solution button so that way others can see the solution.

RS pin of the transceiver connected to PortC pin 1 for can1 and PortC pin 3 is connected to can2 and I made them low using the program. The pins are pulled up by default. I will verify on scope the signals. But at present it is working due to wrong filter configuration, which I have taken from one of the websites.