cancel
Showing results for 
Search instead for 
Did you mean: 

USART INTERRUPT PROBLEM REGISTERS nucleoF303RE

FilipF303RE
Associate III

Hello everyone,

I am struggling with a problem that has not been solved before. Perhaps someone could be found who would be able to solve it. The issue is with the operation of the interrupt for receiving a character via USART. The interrupt is not responding, and I am unable to resolve this problem on my own. The USART transmits and receives the data frame correctly, but when I enable the interrupt for USART reception, it stops receiving. I am trying to control an SG90 servo motor. Its nuclef303RE, MCU stm32f3.

 

#include "stm32f303xe.h"
#include "stdint.h"
#include "stm32f3xx.h"
#include <stdio.h>
#include <string.h>
#define LD4_ON GPIOA -> BSRR |= GPIO_BSRR_BS_5;
#define LD4_OFF GPIOA -> BSRR |= GPIO_BSRR_BR_5;
volatile int currentindex=0;
volatile int position = 1000;
volatile char message;

void clock_config(void)
{
	RCC->CR |= RCC_CR_HSION;
	 while (!(RCC->CR & RCC_CR_HSIRDY));
	 RCC->APB1ENR |= RCC_APB1ENR_PWREN;

	 RCC->CFGR |= RCC_CFGR_HPRE_DIV1;
	 RCC->CFGR|= RCC_CFGR_PPRE1_DIV2;
	 //PPL SOURCE MUX

	// RCC->CFGR |= RCC_CFGR_PLLMUL9;
	 RCC->CFGR |= (0x7 << RCC_CFGR_PLLMUL_Pos);
	 RCC->CR |= RCC_CR_PLLON;
	 while (!(RCC->CR & RCC_CR_PLLRDY));
	 RCC->CFGR |= RCC_CFGR_SW_PLL;
	 while(!(RCC->CFGR & RCC_CFGR_SWS));
}



void config_UART(void)
{
	RCC -> AHBENR |= RCC_AHBENR_GPIOAEN;


	//PA2_TXAF7
	GPIOA -> MODER &= ~(GPIO_MODER_MODER2_0);
    GPIOA->MODER |= GPIO_MODER_MODER2_1;
    GPIOA->AFR[0] &= ~((0xF << GPIO_AFRL_AFRL2_Pos));
	GPIOA->AFR[0] |= (0x7 << GPIO_AFRL_AFRL2_Pos);

	//PA3_RXAF7
	GPIOA -> MODER &= ~(GPIO_MODER_MODER3_0);
	GPIOA->MODER |= GPIO_MODER_MODER3_1;
	GPIOA->AFR[0] &= ~((0xF << GPIO_AFRL_AFRL3_Pos));
	GPIOA->AFR[0] |= (0x7 << GPIO_AFRL_AFRL3_Pos);




	//GPIOA -> OTYPER |= GPIO_OTYPER_OT_3;
	//GPIOA->PUPDR |= GPIO_PUPDR_PUPDR3_0;
	RCC -> APB1ENR |= RCC_APB1ENR_USART2EN;

	//RCC -> CFGR |= RCC_CFGR_PPRE1_2;

	USART2->BRR = 36000000/115200;

	USART2-> CR1 |= USART_CR1_UE | USART_CR1_TE | USART_CR1_RE;
	USART2-> CR1 |= USART_CR1_IDLEIE | USART_CR1_RXNEIE;
	NVIC_SetPriority(USART2_IRQn, 0);
	NVIC_EnableIRQ(USART2_IRQn);



}
void USART2_IRQHandler(void)
{
	if(USART2->ISR & USART_ISR_RXNE)
			{
				message[currentindex] = USART2-> RDR;
				currentindex++;


			}else if(USART2->ISR &  USART_ISR_IDLE)
			{
				if(strcmp(message,"L") == 0)
				{
					if(position < 2000)
					{
						position+=30;
						TIM3->CCR1 = position;
					}
				}
				else if(strcmp(message,"P") == 0)
				{
					if(position > 900)
					{
						position-=30;
						TIM3->CCR1 = position;
					}
				 }
				memset(message,0,currentindex+1);
				currentindex = 0;
				USART2->ICR |= USART_ICR_IDLECF;
			}
	
}


void configureLD4(void)
{

		GPIOA -> MODER |= GPIO_MODER_MODER5_0;
		GPIOA -> MODER &= ~(GPIO_MODER_MODER5_1);
		GPIOA -> OTYPER &= ~(GPIO_OTYPER_OT_5);
		GPIOA -> OSPEEDR &= ~(GPIO_OSPEEDER_OSPEEDR5);
		GPIOA -> PUPDR &= ~(GPIO_PUPDR_PUPDR5);

}


void configureTIMER3(void);
void TIM3_start(void);
void interuptTIM3(void);
void pwmconfigration(void);
void configPWMPA6(void);
int main(void)
{
	
	clock_config();
	configureLD4();
	config_UART();
	configureTIMER3();
	TIM3_start();
	pwmconfigration();
	configPWMPA6();
	interuptTIM3();
	USART2->TDR = 'D';
	while (!(USART2->ISR & USART_ISR_TXE)) { } // Czekaj na opróżnienie bufora
	while (!(USART2->ISR & USART_ISR_TC)) { }  // Czekaj na zakończenie transmisji

	while(1)
	{



	}
}

void configureTIMER3(void)
{
	 //PA6:D12

	RCC -> APB1ENR |= RCC_APB1ENR_TIM3EN;
	TIM3->PSC = 71;   //72mghz
	TIM3->ARR = 19999;  //PA6
}
void TIM3_start(void)
{
	TIM3->CNT=0;
	TIM3->CR1|= TIM_CR1_CEN;
}

void interuptTIM3(void)
{
	TIM3 -> DIER |= TIM_DIER_UIE;
	TIM3 -> DIER |= TIM_DIER_CC1IE;
	NVIC_SetPriority(TIM3_IRQn, 1);
	NVIC_EnableIRQ(TIM3_IRQn);
}
void TIM3_IRQHandler(void)
{
	if(TIM3 -> SR &= ~(TIM_SR_UIF))
	{
		TIM3 -> SR &= ~(TIM_SR_UIF);
	}
	if(TIM3 -> SR & TIM_SR_CC1IF)
		{
			TIM3 -> SR &= ~(TIM_SR_CC1IF);
		}
}
void pwmconfigration(void)
{
	TIM3 -> CCMR1 |= TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_2;
	TIM3 -> CCMR1 |= TIM_CCMR1_OC1PE;
	TIM3 -> CCR1 = 900;
	 TIM3->CR1 |= TIM_CR1_ARPE;
	TIM3 -> CCER |= TIM_CCER_CC1E;
}
void configPWMPA6(void)
{

	GPIOA-> MODER |= GPIO_MODER_MODER6_1;
	GPIOA->AFR[0] |= (0x2 << GPIO_AFRL_AFRL6_Pos);
}

 

 
 
 
 
 
 
1 REPLY 1
AScha.3
Super User

Hi,

did you think on: what, if a receive error coming ? 

USART doing nothing any more, until error state is cleared and again "ready to receive" is set...

+ check in debug, if its coming to the INT, but with any error set...instead of a received byte.

 

btw

i only use the HAL lib, so i cannot tell you, what you should set ; but with HAL also need to handle uart-receive and uart-error, to have it working reliably.

If you feel a post has answered your question, please click "Accept as Solution".