2024-10-03 12:54 PM - edited 2024-10-03 12:58 PM
Hi! I'm working in an application where I want to start a series of ADC conversions every 10 seconds, take a hundred samples and stop the conversions. The way I thought of it is to use a timer (timer 1 in my case) to measure the 10 seconds and use another timer (timer 3) to trigger the ADC conversions. Once the 100 conversions are made, the timer 3 stops until the timer 1 counts to 10 seconds again.
The problem that I have is that the timer 3 does the cycle only one time and after disabling the time base inside the ADC callback function I can't start it again from the TIM1 callback function. This works fine only if I don't use HAL_TIM_Base_Stop(&htim3).
Am I doing something wrong or this method is not possible?
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_9);
HAL_TIM_Base_Start(&htim3);
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, 1);
counter++;
sumVoltage += adcResults[0];
sumBattCurrent += adcResults[1];
if (counter == 100){
voltage = sumVoltage / 100.0 * (3.285 / 4095.0);
battCurrent = ((sumBattCurrent / 100.0) - 3080.0) / 61.0;
counter = 0;
sumVoltage = 0;
sumBattCurrent = 0;
HAL_TIM_Base_Stop(&htim3);
}
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, 0);
}
static void MX_ADC1_Init(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
hadc1.Instance = ADC1;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T3_TRGO;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 3;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_9;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_7CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
sConfig.Rank = ADC_REGULAR_RANK_3;
sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
}
static void MX_TIM1_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
htim1.Instance = TIM1;
htim1.Init.Prescaler = 1835;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 65358;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
}
static void MX_TIM3_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
htim3.Instance = TIM3;
htim3.Init.Prescaler = 0;
htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
htim3.Init.Period = 419;
htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
}
Solved! Go to Solution.
2024-10-03 9:55 PM
> I can't start it again
What is it that you can't start? TIM3 or the ADC conversions? What are exactly the symptoms? What are TIM3 registers content, mainly TIM3_CR1.CEN?
JW
2024-10-03 9:55 PM
> I can't start it again
What is it that you can't start? TIM3 or the ADC conversions? What are exactly the symptoms? What are TIM3 registers content, mainly TIM3_CR1.CEN?
JW
2024-10-04 6:36 AM
Thanks! I'm new to this and don't know much about the registers and low level stuff, with your reply I managed to start the timer 3 and trigger the conversions again after changing the CEN bit in CR1 with TIM3 -> CR1 |= (1 << 0).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.