cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F042F6P7 (TSSPOP20 package): CAN availability on CubeMx

mccabehm
Associate III

Using STM32CubeIDE (v1.14.0) with STM32F042F6P7 (TSSOP 20) to configure CAN pins on custom board. However the CAN peripheral is grayed-out when I open the IOC file in STM32CubeIDE. For pin assignments, PB8 is available for CAN rx but CAN tx is not show for any other pin. How do I access alternate pins for the CAN peripheral? Reference manual says PA12 should be available as alternate for CAN tx; and PA11 should be available as alternate for CAN rx.

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

As stated in the datasheet you need to remap the IOs PA11/12 in place of IO pair PA9/10 using SYSCFG_CFGR1 register:

SofLit_0-1709933856214.png

So in CubeMx go to SYS menu and check the checkbox "Pins PA11/12 instead of pins PA9/10". CAN peripheral will be available.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

2 REPLIES 2
mccabehm
Associate III

I was able to select alternate functions for pins on another STM32 part using <Ctrl + mouse left> when configuring pinout in IOC file. This doesn't appear to be possible with the STM32F042F6P7. Does this mean I can't use the STM32CubeIDE and HAL for the STM32F042F6P7 part?

SofLit
ST Employee

Hello,

As stated in the datasheet you need to remap the IOs PA11/12 in place of IO pair PA9/10 using SYSCFG_CFGR1 register:

SofLit_0-1709933856214.png

So in CubeMx go to SYS menu and check the checkbox "Pins PA11/12 instead of pins PA9/10". CAN peripheral will be available.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.