2024-05-13 08:51 AM
Dear all,
I am trying to convert the SPL to LL using the SPL2LL converter. After pressing the migrate button, I got the message below. Please help. Is it the problem that I chose the wrong directory? I chose the directory where the main.c file is located (./). All the others' ./apps are stored in /app.
2024-05-15 02:08 AM
and what platform you're running on, version, etc ...
2024-05-15 02:13 AM
Dear Andrew and Tesla,
After the SPL2LL conversion, I got the messages below.
Message 1:
[WARNING] -- Line 2096 -- "NVIC_SetVectorTable" No LL API, StdPeriph legacy API is used instead (legacy library)
Message 2:
[WARNING] -- Line 238 -- "I2C_CheckEvent" No LL API exist, migration is ensured by using direct access register
About Message 1, does it mean an API is stored in the legacy folder, and I can use it now without making any manual modifications?
About Message 2, does it mean I don't need to make any modifications manually?
2024-05-15 02:30 AM - edited 2024-05-15 02:31 AM
This is an entirely new question - nothing to do with the original post & title of the thread, "SPL2LL converter error message".
It'd be best to leave this thread for the issues of getting the tool itself to work, and start a new thread for the unrelated issues of how to migrate your specific source code.
Put a link here so people can find the new thread.
2024-05-15 02:45 AM
Dear Andrew,
As I mentioned in the previous message, I am using Perl 5.24.4.1 and running on Windows11 platform.
2024-05-15 02:48 AM
no, you hadn't mentioned Windows 11.
2024-05-15 03:16 AM - edited 2024-05-15 04:01 AM
.