cancel
Showing results for 
Search instead for 
Did you mean: 

SPL2LL converter error message

khwuuk
Associate III

Dear all,


I am trying to convert the SPL to LL using the SPL2LL converter. After pressing the migrate button, I got the message below. Please help. Is it the problem that I chose the wrong directory? I chose the directory where the main.c file is located (./). All the others' ./apps are stored in /app.

khwuuk_1-1715615219213.png

 

 

15 REPLIES 15

>>Is it the problem that I chose the wrong directory? 

I don't know. Try simpler pathing, and perhaps without spaces or special characters.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Tesla DeLorean wrote:

without spaces or special characters.


^^^^ This! Always! ^^^^

@khwuuk  See: 

https://www.avrfreaks.net/s/topic/a5C3l000000UY8vEAG/t145039?comment=P-1182240

 

khwuuk
Associate III

Dear Tesla and Andrew,

 

I removed the space, and no special characters were on the path. There are still error messages.

 

Is it the problem of Strawberry Perl? I installed ActiveState Perl and Strawberry Perl at the same.

khwuuk
Associate III

Dear Tesla and Andrew,

 

After installing the older version of Perl, I can run the SPL2LL converter now.

Thank you so much.

Thanks for updating - please mark that as the solution.

Might also be helpful to mention which version 

khwuuk
Associate III

Dear Tesla and Andrew,

 

I am using the SPL2LL converter's GUI interface. Does the source file path mean the location of the main.c? Or do I need to group all the .c .h files into one folder? Please give me some hints about it.

Thank you very much.

I've never used it, so I have no idea.

However, the errors you posted in the OP don't seem to be about failure to find your source files - they look more like errors in the utility itself.

 

EDIT:

You didn't answer the question of what Perl version you are using.

You should probably also state what platform you're running on, version, etc ...

@STTwo-32 can someone review the status of this tool and what dependencies it has. Perhaps doing a 2024 refresh with current expectations and document them. Thanks.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Dear Andrew,

 

I used the old Perl version. The higher version is not supported.