2014-11-25 2:33 AM
Hi. All!
I want to use FSMC module, but I'm not sure that it settings correct. There is write operation on a picture. I see multiple NWE activation. And sometime it release NEx together NWE (should be NWE and than NEx). What should I do for diagram like Figure 437 from ? Or, possible, I don't understand something?typedef
struct
{
__IO uint8_t data;
} Modem_TypeDef;
#define MDATA ((uint32_t)(0x60000000))
#define MADDR ((uint32_t)(0x60000000 | 0x100))
#define M_DATA ((Modem_TypeDef *) MDATA)
#define M_ADDR ((Modem_TypeDef *) MADDR)
{
initFSMC();
while
(1)
{
GPIO_WriteBit( GPIOE, GPIO_Pin_0, Bit_SET);
//my own strobe
M_DATA->data = 0x77;
M_ADDR->data = 0x33;
GPIO_WriteBit( GPIOE, GPIO_Pin_0, Bit_RESET);
//my own strobe
}
}
void
initFSMC(
void
)
{
// --- initialization FSMC ---
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOE, ENABLE);
//clock for FSMC
RCC_AHB3PeriphClockCmd( RCC_AHB3Periph_FSMC, ENABLE);
// configure GPIOE [4:8]
gpio.GPIO_Mode = GPIO_Mode_AF;
gpio.GPIO_OType = GPIO_OType_PP;
gpio.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11;
gpio.GPIO_PuPd = GPIO_PuPd_UP;
gpio.GPIO_Speed = GPIO_Speed_25MHz;
GPIO_Init( GPIOE, &gpio);
// configure GPIOD [0,1,4,5,7,14,15]
gpio.GPIO_Mode = GPIO_Mode_AF;
gpio.GPIO_OType = GPIO_OType_PP;
gpio.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4 | GPIO_Pin_5 |\
GPIO_Pin_7 | GPIO_Pin_14 | GPIO_Pin_15;
gpio.GPIO_PuPd = GPIO_PuPd_UP;
gpio.GPIO_Speed = GPIO_Speed_25MHz;
GPIO_Init( GPIOD, &gpio);
// timings
modemTimInit_str.FSMC_AddressSetupTime = 0;
// used but don't care
modemTimInit_str.FSMC_AddressHoldTime = 0;
// don't used
modemTimInit_str.FSMC_DataSetupTime = 5;
modemTimInit_str.FSMC_BusTurnAroundDuration = 0;
// don't used
modemTimInit_str.FSMC_CLKDivision = 2;
modemTimInit_str.FSMC_DataLatency = 0;
// don't used
modemTimInit_str.FSMC_AccessMode = FSMC_AccessMode_A;
FSMC_NORSRAMStructInit( &modemInit_str);
// Apply default values
// Reset NOR/SRAM Initialization structure parameters values
modemInit_str.FSMC_Bank = FSMC_Bank1_NORSRAM1;
modemInit_str.FSMC_DataAddressMux = FSMC_DataAddressMux_Enable;
modemInit_str.FSMC_MemoryType = FSMC_MemoryType_PSRAM;
//FSMC_MemoryType_SRAM;
modemInit_str.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_8b;
modemInit_str.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable;
modemInit_str.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable;
modemInit_str.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
modemInit_str.FSMC_WrapMode = FSMC_WrapMode_Disable;
modemInit_str.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;
modemInit_str.FSMC_WriteOperation = FSMC_WriteOperation_Enable;
modemInit_str.FSMC_WaitSignal = FSMC_WaitSignal_Disable;
modemInit_str.FSMC_ExtendedMode = FSMC_ExtendedMode_Enable;
//FSMC_ExtendedMode_Disable;
modemInit_str.FSMC_WriteBurst = FSMC_WriteBurst_Disable;
modemInit_str.FSMC_ReadWriteTimingStruct = &modemTimInit_str;
modemInit_str.FSMC_WriteTimingStruct = &modemTimInit_str;
GPIO_PinAFConfig(GPIOE, GPIO_PinSource7, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource8, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource9, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource10, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource11, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource7, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_FSMC);
FSMC_NORSRAMInit( &modemInit_str);
FSMC_NORSRAMCmd( FSMC_Bank1_NORSRAM1, ENABLE);
}
#stm32f4 #fsmc #sram
2014-11-25 10:19 AM
At 24 Msamples per second you are probably not capturing single write pulses - if you run the mcu at 168MHz, they should last around 40ns. Show us also the capture of your ''marker'' signal, not hand-drawn lines.
Also, I don't speak the library gobbledygook, but it appears to me that you set FSMC for multiplexed memory but you don't initialize FSMC_NL, I suspect you do this in error. JW2014-11-25 6:55 PM
Thank you! You was right - samplerate was too low. It worked on default frequency - 16MHz HSI (not 168MHz, of course! ), but samples couldn't show all details. For 16MHz need 32MHz sample frequency minimum (as told Nyqist and Kotelnikov).
I addedRCC_HCLKConfig( RCC_SYSCLK_Div4);
// make it slow
and now I have this one. Black - NEx,red
- NWE,brown
- soft strobe (see source upper):2014-11-26 10:29 AM
> now I have this one
And what's wrong with it?
> Can you explain it more detail? What means 'multiplexed' for FSMC? In my appinion, it means that data and address used the same wires. Roughly, yes. So, you need some way to distinguish between data and address. That is the purpose of FSMC_NL - it is supposed to drive a latch which latches the addresses before data are read/written. Read the manual. > I don't need it really. Now I want to use just A8 bit. Then don't use the multiplexing mode. JW
2014-11-26 11:54 PM
I can't do it still! Agrh...
So, I need ModeA or ModeD. It means, I should use extended mode and write timings in both BTR1 and BWTR1 ( bank 1 for NOR/PSRAM). I declare structure for IO:#define
M_BASE ((uint32_t)(0x60000000))#define
MADDR ((uint32_t)((0x60000000 | 0x100)-4))#define
M_ADDR ((Modem_TypeDef *) MADDR) So, now I can write there:for (i=0;i<8;i++) {
M_ADDR->data[i] = i; } and listing:80004a8: 2300 movs r3, #0
for (i=0;i<8;i++) { M_ADDR->data[i] = i; 80004aa: 4a07 ldr r2, [pc, #28] ; (80004c8 <main+0x88>) 80004ac: b2d9 uxtb r1, r3 80004ae: 54d1 strb r1, [r2, r3] 80004b0: 3301 adds r3, #1 for (i=0;i<8;i++) { 80004b2: 2b08 cmp r3, #8 80004b4: d1f9 bne.n 80004aa <main+0x6a> 80004b6: e7ef b.n 8000498 <main+0x58> 80004c8: 600000fc .word 0x600000fc For use this opportunity request initialize FSMC module: clock, gpio, connect pins to alternate function.void
initFSMC(
void
)
{
FSMC_NORSRAMInitTypeDef modemInit_str;
FSMC_NORSRAMTimingInitTypeDef modemTimings;
// --- initialization FSMC ---
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOE | RCC_AHB1Periph_GPIOB, ENABLE);
//clock for FSMC
RCC_AHB3PeriphClockCmd( RCC_AHB3Periph_FSMC, ENABLE);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource7, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource8, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource9, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource10, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource11, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource12, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource13, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource14, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource15, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource7, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource10, GPIO_AF_FSMC);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_FSMC);
// configure GPIOE [4:8]
gpio.GPIO_Mode = GPIO_Mode_AF;
gpio.GPIO_OType = GPIO_OType_PP;
//gpio.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11;
gpio.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | \
GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;
gpio.GPIO_PuPd = GPIO_PuPd_UP;
gpio.GPIO_Speed = GPIO_Speed_25MHz;
GPIO_Init( GPIOE, &gpio);
// configure GPIOD [0,1,4,5,7,14,15]
gpio.GPIO_Mode = GPIO_Mode_AF;
gpio.GPIO_OType = GPIO_OType_PP;
//gpio.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_7 | GPIO_Pin_14 | GPIO_Pin_15;
gpio.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_7 | GPIO_Pin_14 | GPIO_Pin_15 | \
GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10;
gpio.GPIO_PuPd = GPIO_PuPd_UP;
gpio.GPIO_Speed = GPIO_Speed_25MHz;
GPIO_Init( GPIOD, &gpio);
// configure GPIOB [7]
gpio.GPIO_Mode = GPIO_Mode_AF;
gpio.GPIO_OType = GPIO_OType_PP;
gpio.GPIO_Pin = GPIO_Pin_7;
gpio.GPIO_PuPd = GPIO_PuPd_UP;
gpio.GPIO_Speed = GPIO_Speed_25MHz;
GPIO_Init( GPIOB, &gpio);
// over Register
// Timings MODE A
//ACCMOD BUSTURN DATAST ADDHLD
// || |||| | | | | ADDSET
// 33 22 2222 2222 1111 111111 | | |
// 10 98 7654 3210 9876 54321098 7654 3210
// oo 00 oooo oooo 0000 00000101 oooo 0011 BTR1,BWTR=0x00000503
FSMC_Bank1E->BWTR[0]=(uint32_t) 0x0503;
//WriteMode timings
FSMC_Bank1->BTCR[1]=(uint32_t) 0x0503;
//ReadMode timings
// EXTMOD WREN MTYP[SRAM|PSRAM|NOR]
// | | MWID[8|16] || MUXEN
// 332222222222 1 111 1 1 1 1 1 1 || || | MBKEN
// 109876543210 9 876 5 4 3 2 1 0 9 8 7 6 54 32 1 0
// oooooooooooo.0 000.0 1 0 1.o 0 o 0.l o 00.01 0 1 BCR1=0x0000 5085
FSMC_Bank1->BTCR[0]=(uint32_t) 0x5085;
}
It is works but not full!
As I know, pin PE11 (DA8) must be output for the lowest address bit when I select MUXEN=0x0 and MWID=0x0 (equ 8bit). Right?
But logic analyser show me - wire doesn't changed! In multiplexed mode it changed address but started value is 'full in 1', then 00, 01,... I haven't idea anymore!
2014-11-27 5:53 AM
People, who have english as native language, please, check details in Table 218 on RM0090 and explain me - can I use SRAM/PSRAM in 8 bit read-write mode?
2014-11-27 10:30 AM
That has nothing to do with English; it's simply a prime example of the inferior quality of STM32 documentation.
Note, that that table's title is ''example of supported memories and transactions''. I guess it comes from some preliminary internal/promo material to the FSMC IP module, and IMO it should've never appeared in the manual, and serves only to confusion. Of course you can use 8-bit SRAM. JW2014-11-27 7:18 PM
Thank you, Jan.
I asked about ''Memory data width'' column - what it means? Why is it always 16? Should I use only 16bit SRAM? Or I should separate low and high byte over NBL? One more moment - I forgot check some details in datasheet. 407VG hasn't lower adress lines, because it hasn't port F and G. Sorry... I agree - ST document style isn't easy to understand. For example - TI is better. But their chip is more expensive (for me only, maybe).2014-11-27 11:38 PM
So, how to connect 8bit device like SRAM?
Firstly, see a Table ''FSMC pin definition''. I didn't do it at first - it was my mistake. If your chip hasn't some pin - you can't use these signals. For 407VG and SRAM you hasn't address line A[15:0]. Initialise requested pins D[7:0], NEx, NOE, NWE A[max:16] and other if you need as described in ''stm32f4xx_fsmc.c'' (strange place, imho). And when you write or read your device - you should calculate address as MEMBASE+(ADDR<<n), where MEMBASE = 0x60000000 for SRAM/PSRAM/NOR bank, ADDR = byte's address in your device, n =17. b.r., Oleg