cancel
Showing results for 
Search instead for 
Did you mean: 

TEC CAN error instantly full

zamolan
Associate II
Posted on November 27, 2014 at 20:31

Hi all! 

  In what cases will the Transmit Error Counter register jump from 0 to 0xF8? I am debugging this CAN transmission sequence, and after the Transmit request is set, the next step in debug will show a full ESR : 0x00F80057.

  Is this meaning an incomplete configuration of CAN module and GPIO Pin? Or a nonfunctional CAN Transceiver?

   I would be more than happy if you can give me a hint on it. 

I have attached the registerlayout screenshot of the CAN1 module after the debugger left the CANTransmit() function. 

  

#can #tec-register
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0