cancel
Showing results for 
Search instead for 
Did you mean: 

SD card to USB data Copy using the CH376s IC

YShah.1
Associate II

Hello,

 

I am Use the STM32F091 controller Now we are facing issue on data copying from SD card to USB pendrive.

error is "No Free Sector available" Ping is ok, File is open all are ok only problem on last phase How to resolve that ? Please suggest me.

 

We are use the Ready Library of CH376 and Also Uart of our MCU use are UART5 Number 

USB IC: CH376s 

MCU : STM32F091

 

 

 

Regards

Yash Shah

4 REPLIES 4
FBL
ST Employee

Hi @YShah.1 

Did you try to format your SD card?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

Thanks For Reply I Am Not try the Format of SD card using The Hard card reader Is it Problem Like that ?

I was Format The Pendrive.

 

Perhaps there is a site or venue more suitable for the discussion and debugging of issues with the CH376 device?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

SD Card Format manually but problem as it is