2024-01-08 7:26 AM - last edited on 2024-01-23 4:50 AM by Imen.D
Hello,
I have this code
// Initialiser le bloc A
fresult= HAL_SAI_Init(&hsai_BlockA1);
if (fresult != HAL_OK)
{
return HAL_ERROR;
}
// Initialiser le bloc B
fresult= HAL_SAI_Init(&hsai_BlockB1);
if (fresult != HAL_OK)
{
return HAL_ERROR;
}
// Transmission
fresult = HAL_SAI_Transmit(&hsai_BlockB1, (uint8_t *)playbuf, (sizeof(playbuf))/4, 0xFF);
if (fresult != HAL_OK)
{
return HAL_ERROR;
}
// Reception
fresult = HAL_SAI_Receive(&hsai_BlockA1, (uint8_t *)playbuf_RX, (sizeof(playbuf_RX))/4, 0xFF);
if (fresult != HAL_OK)
{
return HAL_ERROR;
}
I am not receiving some of the data, do you know where I can find the documentation to implement SAI blocking mode? thanks in advance.
In my reception array I have only a part of data, and yet my TX table is well initialized like this :
2024-01-18 6:26 AM
> My CPU clock is 16 MHz
Not, it probably does not.
Don't stop looking and thinking just because you found one number.
HSI = internal RC oscillator is the clock source.
Which then goes through the PLL, with PLLM as the first divider, as can be seen in the little pic you posted.
You really need to "go to school" and / or read / watch lots of basic stuff, about the basics of programming in C, controllers, and probably electronics in general.
I'm out for now, sorry.
2024-01-18 6:34 AM
In any case, thank you for your advice. It's a little late for me to go to school.
2024-01-18 7:54 AM
What I meant is to learn more basics, read and watch basic tutorials, ask colleagues, friends, whatever.
Right now you're kind of running through the dark, no offense meant, everybody has to start somewhere. And an STM32 is quite a big challenge for a beginner.
2024-01-18 8:04 AM
You've already helped me a lot and I thank you very much. I'll follow your advice. Only reading the datasheets or watching the tutorials is not a good method (I2S#SAI, not the same µP, not the same function prototypes....) I need examples and practice to realize that it's not as simple as that. But I've no choice, this SAI part has to work !
2024-01-22 7:21 AM - edited 2024-01-22 7:30 AM
Hi,
After decreasing the size of the table to 128, and modify the DMA configuration for TX and RX like this :
In the Main I have something like this :
while (1)
{
/* USER CODE END WHILE */
if( dataReadyFlag_1)
{
processData_1();
}
if( dataReadyFlag_2)
{
processData_2();
}
/* USER CODE BEGIN 3 */
}
And in the processData_1(); I fill half of the table and the same for the second half of the table.
void processData_1 ()
{ for (int32_t n=0; n<(BUFFER_SIZE/2); n++)
{checkbuf_RX[n]=playbuf_RX[n];}
dataReadyFlag_1=0;
}
For the processing time I am on time. With 110 MHz (time of a clock cycle). I'll have
2x128x1/(110.10e -6) = 2.3µs x 4 (factor) = 9.3 µs which is less than 27µs. But I have only half of the data, looks like the other half is not working. I certainly forgot a few things but what ?
And yet my TX table is correct
For the scope I have (yellow : data. blue : FS)
2024-01-22 7:32 AM
Show the function processData_2(), it should look something like this:
void processData_2()
{ for( int32_t n = (BUFFER_SIZE / 2); n < BUFFER_SIZE; n++ )
{
checkbuf_RX[n]=playbuf_RX[n];
}
dataReadyFlag_2 = 0;
}
2024-01-22 7:34 AM - edited 2024-01-22 7:40 AM
I think it's the same
void processData_2 ()
{
for (int32_t n=64; n<BUFFER_SIZE; n++)
{
checkbuf_RX[n]=playbuf_RX[n];
}
dataReadyFlag_2=0;
}
And the callback :
void HAL_SAI_RxHalfCpltCallback (SAI_HandleTypeDef *hsai)
{
dataReadyFlag_1=1;
}
void HAL_SAI_RxCpltCallback (SAI_HandleTypeDef *hsai)
{
dataReadyFlag_2=1;
}
2024-01-22 9:18 AM
> I think it's the same
Probably yes. Be more consistent, which means: don't use a number, and then a define - I mean the "64".
And for incrementing always use unsigned integers (uint32_t in this case).
To check that both flags are set: in processData_1() (better call it "half" or so than "1") set a GPIO high, in processData_2() (better call it "full" or so than "2") set the same GPIO low again. If both flags are set and reset again, the GPIO should toggle with a rate equal to sampling rate / buffer size. Check with scope.
2024-01-24 1:58 AM - edited 2024-01-24 4:17 AM
Hi,
I'll come back with the curves.The result is not there but I have values.
yellow :FS / blue : led flashing
My sample rate is 44.1 kHz (real : 35.7 kHz). So sampling rate/128 = 278 Hz (about), but I have 571 Hz (about twice as much). I'm Debug mode and maybe in Release mode that would change something ?