Question
RTC Wakeup Interrupt not working on STM32H7 dual-core MCU
Hello everybody,
I'm using STM32CubeIDE version v1.7.0 and Firmware package FW_H7 v1.9.0.
The tests were made on a Nucleo H745ZI (dual-core MCU).
Test 1:
- Enabled RTC for the M7
- Configured RTC Wakeup parameters
- Enabled RTC Wakeup interrupt on NVIC
Result: The RTC Wakeup interrupt is not firing!
Test 2:
- Enabled RTC for the M4
- Configured RTC Wakeup parameters
- Enabled RTC Wakeup interrupt on NVIC
Result: The RTC Wakeup interrupt is not firing!
Made the same test configuration on a Nucleo H743ZI (single-core MCU) and there the RTC Wakeup interrupt is firing! (At least there 8))
Any ideas?