2025-01-24 11:19 PM - last edited on 2025-01-25 09:07 AM by SofLit
Hello STM,
I'm working on a project using the STM32H7R3L8H6H MCU with a PSRAM chip connected via HEXASPI to XSPM1. I'm encountering massive issues with the PSRAM initialization, which I described in a different post. I found a discrepancy between the RM0477 Reference manual documentation and the STM32CubeProgrammer during my tests.
The XSPI_TCR register is described like this in the RM0477:
If I open the STM32CubeProgrammer register window, I find a DHQC flag on the register bit 28 position.
This bit is set to 1 all the time, and I have no information about its meaning.
Can someone please explain the function of this flag?
The STM32H7Rx/7Sx Arm®-based 32-bit MCUs are somewhat complex devices, and one would expect an actual reference manual. This isn't just some kind of "typo" in the documentation; it's another flag that probably has some functionality attached to it.
Be vigilant and always remember:
"Always be yourself. Unless you can be a pirate. Then always be a pirate."
2025-01-27 02:00 AM
Hello @Intector ,
Thank you for bringing this issue to our attention.
I reported this issue internally. And, I will come back to you with details as soon as possible.
Internal ticket number: 201430 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.