cancel
Showing results for 
Search instead for 
Did you mean: 

RM0440, Rev 6, STM32G4 Reference Manual - Errors

Singh.Harjit
Senior II
  1. Figure 151, Page 682: The second line in the picture should be "ADC Master EOC".
  2. Section 27.5.68, Page 1054: Description for bit 20 ADCTBRST should be similar to bit 14. Currently, it is a circular reference to itself "Refer to ADC3TBRST description." :^)
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Igor Cesko
ST Employee

Hi Singh.Harjit,

Thanks for info - it will be corrected in next revision.

Regards

Igor