cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with RDP regression

Istillaga
Senior

Hi

When I was returning from RDP level 1 to 0 the stm32cube programmer program crashed and now every time I try to access the microcontroller several different cases happen:

1- Connect and instantly lose the connection giving the next error: Error: Data read failed
2-Cannot connect to access port 0! If you are trying to connect to a device with TrustZone enabled, try connecting with HotPlug mode. If you are trying to connect to a device that supports debug authentication with a certificate or password, open your device using it.
3- Detects the id 0x00 when it should be 0x482, Error: Unable to get core ID

 

2 REPLIES 2
Imen.D
ST Employee

Hello @Istillaga,

I advise you to review and follow this FAQ and post:

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Jeff Tenney
Senior

Hi @Istillaga did you resolve this issue?  I'm having the same problem - but I was disabling TZ when stm32cube programmer had an error.