2024-05-15 01:44 AM - edited 2024-05-15 01:45 AM
Hi
When I was returning from RDP level 1 to 0 the stm32cube programmer program crashed and now every time I try to access the microcontroller several different cases happen:
1- Connect and instantly lose the connection giving the next error: Error: Data read failed
2-Cannot connect to access port 0! If you are trying to connect to a device with TrustZone enabled, try connecting with HotPlug mode. If you are trying to connect to a device that supports debug authentication with a certificate or password, open your device using it.
3- Detects the id 0x00 when it should be 0x482, Error: Unable to get core ID
2024-05-16 07:59 AM
Hello @Istillaga,
I advise you to review and follow this FAQ and post:
2024-05-25 01:25 PM
Hi @Istillaga did you resolve this issue? I'm having the same problem - but I was disabling TZ when stm32cube programmer had an error.