cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with data reception via USART3 on STM32F429-Disco board

Emanuele78
Associate III

Original post: https://community.st.com/t5/stm32cubemx-mcus/problems-with-data-reception-via-usart2-on-stm32f429zi/td-p/741765

Even setting USART3 it doesn't work (see attachments). Did I make a mistake setting some parameters, or is something missing? Thanks a lot

14 REPLIES 14

@mƎALLEm wrote:

From the user manual of the board


@mƎALLEm  This is another case where the Hardware block diagram (Fig 2) in the UM could be more helpful:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/nucleo-user-manuals-don-t-show-the-vcp-uart-connection/td-p/644955

AndrewNeil_0-1731411329320.png

 

Already mentioned in the User manual of the board:

SofLit_1-1731409358224.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Is this a new board?

Because older revisions (B01) of it did not have the VCP capability.

Revision should be displayed on a sticker on the bottom of the board.

JW

Yes, but it would be more helpful if it were also shown in the block diagram.


@waclawek.jan wrote:

older revisions (B01) of it did not have the VCP capability.


I guess that's why it's not shown on the block diagram - it was just copied without being updated?