2024-11-12 2:22 AM - last edited on 2024-11-12 2:37 AM by mƎALLEm
Original post: https://community.st.com/t5/stm32cubemx-mcus/problems-with-data-reception-via-usart2-on-stm32f429zi/td-p/741765
Even setting USART3 it doesn't work (see attachments). Did I make a mistake setting some parameters, or is something missing? Thanks a lot
Solved! Go to Solution.
2024-11-12 3:35 AM
@mƎALLEm wrote:From the user manual of the board
@mƎALLEm This is another case where the Hardware block diagram (Fig 2) in the UM could be more helpful:
2024-11-12 3:39 AM
Already mentioned in the User manual of the board:
2024-11-12 4:02 AM
Is this a new board?
Because older revisions (B01) of it did not have the VCP capability.
Revision should be displayed on a sticker on the bottom of the board.
JW
2024-11-12 4:11 AM
Yes, but it would be more helpful if it were also shown in the block diagram.
2024-11-20 1:32 AM
@waclawek.jan wrote:older revisions (B01) of it did not have the VCP capability.
I guess that's why it's not shown on the block diagram - it was just copied without being updated?