2024-06-26 05:23 AM
Hi,
I have two MCU communicating with each other via RS485. It's a very simple code one MCU send a data to other and the other is trying to receive this.
With MCU2 code everything is fine. It sends data like it should be.
Problem is with MCU1 code. When I delete #65 line in code (that one with HAL_UART_Transmit...) it works great. It receive data from MCU2 and starts engine and horn. But when I add this line it stop working. I dont understand why this is happening.
When the MCU2 works as a receiver everything is ok, but when I try to send something from it suddenly the whole uart stops working
MCU1 code:
/* USER CODE BEGIN 0 */
uint8_t buffer[2];
uint8_t ZERO[2]={0x00,0x00};
uint8_t AA[2]={0xAA,0xAA};
uint8_t BB[2]={0xBB,0xBB};
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if(buffer[0]==0xCC && buffer[1]==0xCC)
{
Engine(ON);
}
if(buffer[0]==0xDD && buffer[1]==0xDD)
{
Horn(ON);
}
HAL_UART_Receive_IT(&huart2, buffer, 2);
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
//MX_I2C1_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
transceiver(WRITE);
HAL_UART_Transmit(&huart2, ZERO, 2, 10);
transceiver(READ);
HAL_UART_Receive_IT(&huart2, buffer, 2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
MCU2 code:
/* USER CODE BEGIN 0 */
uint8_t CC[2]={0xCC,0xCC};
uint8_t DD[2]={0xDD,0xDD};
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
HAL_Delay(1000);
transceiver(WRITE);
HAL_UART_Transmit(&huart2, CC, 2, 10);
HAL_Delay(1000);
HAL_UART_Transmit(&huart2, DD, 2, 10);
transceiver(READ);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
Solved! Go to Solution.
2024-06-28 09:30 AM
Ok, so i tried with HAL_UART_Transmit_IT but it didnt work.
By accident I disconnected my oscilloscope from MCU1 UART lines and now it works.
2024-06-26 07:56 AM
Instrument the code so you have some idea as to what's going on
Does HAL_UART_Receive_IT() return an error in any of these case?
Is there an error or status flagged by the UART that needs to be cleared for reception to work? Are you clearing it?
2024-06-26 11:15 AM - edited 2024-06-26 11:15 AM
You don't check for HAL status on any of the HAL calls so how do you know what is happening?
if(HAL_UART_Transmit(&huart2, ZERO, 2, 10) != HAL_OK)
{
// Do some error handling
}
if(HAL_UART_Receive_IT(&huart2, buffer, 2) != HAL_OK)
{
// Do some error handling
}
And what do these do?
transceiver(WRITE);
transceiver(READ);
2024-06-27 06:59 AM
I modified MCU1 code a little bit.
/* USER CODE BEGIN 0 */
uint8_t buffer[2];
uint8_t ZERO[2]={0x00,0x00};
uint8_t AA[2]={0xAA,0xAA};
uint8_t BB[2]={0xBB,0xBB};
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if(buffer[0]==0xCC && buffer[1]==0xCC)
{
LED1(ON);
}
if(buffer[0]==0xDD && buffer[1]==0xDD)
{
LED2(ON);
}
if(buffer[0]==0xEE && buffer[1]==0xEE)
{
LED1(OFF);
LED2(OFF);
}
if((HAL_UART_Receive_IT(&huart2, buffer, 2))==!HAL_OK)
{
LED3(ON);
}
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
//MX_I2C1_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
transceiver(WRITE);
if((HAL_UART_Transmit(&huart2, ZERO, 2, 10))==!HAL_OK)
LED3(ON);
transceiver(READ);
HAL_UART_Receive_IT(&huart2, buffer, 2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
On MCU2 I have 3 switches. When I push down first switch it sends {0xCC,0xCC}, second switch {0xDD,0xDD} and third switch {0xEE,0xEE}.
LED3 is off, so everytime status of HAL_UART_Transmist and HAL_UART_Receive_IT is HAL_OK.
Something I saw is that if I press the button once, LED 1 or 2 doesn't light up, but if I press it twice, it does. In the same way to off the LEDs I need two presses.
It's as if HAL_UART_Receive_IT is configured to a 4 byte buffer and not a 2 byte buffer.
2024-06-27 07:10 AM
You still didn't answer my last question
2024-06-27 07:19 AM
@Raf_al wrote:On MCU2 I have 3 switches. When I push down first switch it sends {0xCC,0xCC}, second switch {0xDD,0xDD} and third switch {0xEE,0xEE}..
Are your switches debounced ?
2024-06-27 07:19 AM
Right,
transceiver(WRITE); transceiver(READ);
That just sets the state of the rs485 transceiver.
Transceiver (WRITE) sets 1 on the pin to send data
Transceiver (READ) sets 0 on the pin to receive data
Generally this function works well I looked it up on an oscilloscope.
2024-06-27 07:20 AM
@Raf_al wrote:With MCU2 code everything is fine. It sends data like it should be.
How have you proved that?
2024-06-27 07:27 AM
Yes
2024-06-27 07:29 AM
I can see on the oscilloscope that it sends, for example, these {0xDD,0xDD} when I press the button. I just decode the whole frame. It's simple UART 8n1