Problem with Timer2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 3:40 AM
Hi
I have am using the Timer2 on the STM32L433 chip, and for some reason the interupt gets called as soon as timer is started. Below is my code, and the clocks are running at 60MHz. Anyone any idea what I have done wrong?
Many Thanks
Scott.
void main(void)
{
.....
Timer2_Init();
Start_OneShotTimer2(3000); //set for 3 seconds, but interupt routine gets called straight away
while(1){}
}
void Timer2_Init(void)
{
// Enable Timer 2 clock
RCC->APB1ENR1 |= RCC_APB1ENR1_TIM2EN;
// Configure the timer for one-pulse mode
TIM2->CR1 |= TIM_CR1_OPM; // One-Pulse Mode (counter stops after update event)
// Enable TIM2 interrupt in NVIC
NVIC_EnableIRQ(TIM2_IRQn);
}
void Start_OneShotTimer2(uint32_t milliseconds)
{
uint32_t prescaler;
// 1. Stop the timer before modifying its configuration
TIM2->CR1 &= ~TIM_CR1_CEN; // Stop the timer (disable counter)
// 2. Clear any previous interrupt flags
TIM2->SR = 0; // Clear all status flags, including UIF
// 3. Disable the interrupt while configuring the timer
TIM2->DIER &= ~TIM_DIER_UIE; // Disable the update interrupt
// 4. Calculate the prescaler (prescale to 1 µs)
TIM2->PSC = 59999; // Set the prescaler for 1 µs ticks
// 5. Set the auto-reload value for the desired delay (milliseconds converted to µs)
uint32_t arr = (milliseconds * 1000) - 1; // Convert ms to µs
TIM2->ARR = arr; // Set auto-reload value
// 6. Reset the counter to ensure it starts from 0
TIM2->CNT = 0; // Reset the counter value
// 7. Enable the update interrupt (only now)
TIM2->DIER |= TIM_DIER_UIE; // Enable the update interrupt
// 8. Start the timer
TIM2->CR1 |= TIM_CR1_CEN;
}
void TIM2_IRQHandler(void)
{
if (TIM2->SR & TIM_SR_UIF)
{ // Check for the update interrupt flag
TIM2->SR &= ~TIM_SR_UIF; // Clear the interrupt flag
.......
}
}
- Labels:
-
STM32F4 Series
-
STM32L4 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-16 10:24 AM
Hello @SSmit.13
Try adding a delay before starting the timer to ensure that all configurations are correctly applied.
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-16 10:58 AM
TIMx_PSC is preloaded, so the first timer period after enabling it is with the original prescaler value, which by default is 0.
You can force update (which would load the preloaded PSC value into the real PSC register) by setting TIMx_EGR.UG.
Note that that will set the TIMx_SR.UIF flag, so you have to clear it before enabling the interrupt in TIMx_DIER. Alternatively (and possibly better), use TIMx_CR1.URS to avoid TIMx_SR.UIF being set through setting TIMx_EGR.UG.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-17 1:17 AM
Hi JW
Many thanks for your reply. I added the line for setting the TIM2_EGR.UG , and cleared the TIM2_SR.UIF flag, see below up date. But still the interupt routine is called straight after enabled. Any idea what I am doing wrong?
Thanks
Scott
void Timer2_Init(void)
{
RCC->APB1ENR1 |= RCC_APB1ENR1_TIM2EN;
// Ensure TIM2 is reset
TIM2->CR1 = 0x0000; // Reset control register
TIM2->CR2 = 0x0000; // Reset control register 2
TIM2->DIER = 0x0000; // Reset interrupt enable register
TIM2->SR = 0x0000; // Clear status register
// Enable TIM2 interrupt in NVIC
NVIC_EnableIRQ(TIM2_IRQn);
NVIC_SetPriority(TIM2_IRQn, 1);
}
void Start_OneShotTimer2(uint32_t milliseconds)
{
// Disable TIM2 to configure it
// Disable TIM2 to ensure clean configuration
TIM2->CR1 = 0; // Reset the control register
TIM2->CR1 |= TIM_CR1_OPM; // Enable One-Pulse Mode
TIM2->CR1 |= TIM_CR1_URS; // Only overflow/underflow generates an update interrupt
// Disable update events during configuration
TIM2->CR1 |= TIM_CR1_UDIS;
// Set the Auto-Reload Register (ARR) for the desired delay in milliseconds
TIM2->ARR = milliseconds * 1000 - 1; // Convert ms to µs (1 ms = 1000 µs)
// Configure prescaler for 1 µs resolution (16 MHz / 1 MHz - 1)
TIM2->PSC = 59999;
// Reset the counter to ensure a clean start
TIM2->CNT = 0;
TIM2->EGR = TIM_EGR_UG; << Added here
// Re-enable update events
TIM2->CR1 &= ~TIM_CR1_UDIS;
TIM2->CR1 |= TIM_CR1_DIR;
// Clear the update interrupt flag
TIM2->SR &= ~TIM_SR_UIF;
// Enable update interrupt
TIM2->DIER |= TIM_DIER_UIE;
// Start the timer
TIM2->CR1 |= TIM_CR1_CEN;
}
void TIM2_IRQHandler(void)
{
if (TIM2->SR & TIM_SR_UIF)
{ // Check for the update interrupt flag
TIM2->SR &= ~TIM_SR_UIF; // Clear the interrupt flag
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-17 1:18 AM
Hi Imen
Added a short delay (and tried longer), but no luck.
Cheers
Scott
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-18 6:04 AM
> But still the interupt routine is called straight after enabled
How do you know? How do you observe this?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-18 6:35 AM
An article on Timers that may help