2019-04-05 07:55 AM
I want to connect the PF1-OSC_OUT pin to another circuit on my board, to use this 32.768kHz clock for another counter. ( instead of adding another crystal )
Would this be a problem? I can buffer it to minimize pulling the crystal. Any suggestions?
(I've never attempted this on a STM32 part)
Thanks
Solved! Go to Solution.
2019-04-05 08:03 AM
Yes, that is a problem. There is no loading allowed on the OSC pin beside the crystal and the loading capacitors. Waveforms are also far from "digital". Route LSE to MCO!
2019-04-05 08:03 AM
Yes, that is a problem. There is no loading allowed on the OSC pin beside the crystal and the loading capacitors. Waveforms are also far from "digital". Route LSE to MCO!
2019-04-05 08:22 AM
Thanks for the pointer. Neat feature, But MCOSEL is reset to 0000 0000, resulting in no clock out at reset. Unfortunately this does not work for me. ( I need a clock regardless of system reset)
I'll just add another crystal or resonator.
Thanks
2019-04-05 10:04 AM