cancel
Showing results for 
Search instead for 
Did you mean: 

Only half of the pins are getting declared in CubeIDE

surrvesh
Associate II

While creating new project and initialising the peripherals in default mode , even after doing these the pins are not getting declared default

7 REPLIES 7

Please explain what you mean by this - show examples.

Note that only pins configured as GPIO tend to get their own _GPIO_PIN_ & _GPIO_Port_  definitions; pins used as Alternate Functions (eg, UART Rx & Tx) tend to be handled by the peripheral - so you may not see separate  _GPIO_PIN_ & _GPIO_Port_  definitions for them ...

 

Please use this button to properly post source code:

AndrewNeil_0-1709381124608.png

 

 

Why do you expect that "all" pins of a package are initialized (by CubeMX generated code)?
All pins after a reset will go anyway to their default state (mainly floating, not enabled for "anything").

To be honest: I do not care if pins have to be configured after a reset when I will not use them afterwards. I leave all not used stuff, esp. not used pins, in their "default" state after reset. I have never realized any issue with this approach.

What is your understanding of "default" states of pins? If you mean, "pins have to be brought to their default state" after reset - it is not true. They have a default state with reset done.

surrvesh
Associate II

00:53:41 **** Build of configuration Debug for project project1 ****

make -j12 all

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.o"

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.c:517:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.c:35:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.c:21:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.c:33:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.c:118:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.c:87:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.c:84:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.c:108:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.c:294:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.c:187:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.c:178:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.c:86:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.o] Error 1

make: *** Waiting for unfinished jobs....

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.o] Error 1

"make -j12 all" terminated with exit code 2. Build might be incomplete.

 

00:53:44 Build Failed. 25 errors, 0 warnings. (took 3s.134ms)
im getting this error for any code i write

Hello @surrvesh 

I think you are tooking about the same issue on this post. Can you give more details about your configurations.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

What is your question?

Have you realized your compile error?
../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

Fix this error first (potentially missing files or project include paths are not set properly).
How is it related to your topic as "Only half of the pins are getting declared in CubeIDE"?

Were you every able to compile and flash a FW?

i just installed cube ide and initialized ports for my H653ZI board and created IOC file but not able to build projects in it getting these errors

 

 

 

 

12:21:50 **** Build of configuration Debug for project project1 ****

make -j12 all

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.o"

arm-none-eabi-gcc "../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DUSE_HAL_DRIVER -DSTM32H563xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.d" -MT"Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.o"

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.c:86:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.c:35:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.c:294:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

compilation terminated.

compilation terminated.

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.c:84:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

compilation terminated.

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.c:517:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.c:178:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.c:187:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.c:87:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.c:118:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.c:33:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.c:108:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,

from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.c:21:

../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory

409 | #include "stm32h5xx_hal_usart.h"

| ^~~~~~~~~~~~~~~~~~~~~~~

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.o] Error 1

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

make: *** Waiting for unfinished jobs....

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_exti.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_adc_ex.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_flash_ex.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_dma_ex.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth_ex.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_gpio.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_eth.o] Error 1

make: *** [Drivers/STM32H5xx_HAL_Driver/Src/subdir.mk:100: Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal_cortex.o] Error 1

"make -j12 all" terminated with exit code 2. Build might be incomplete.

 

12:21:51 Build Failed. 25 errors, 0 warnings. (took 939ms)

 

 


@surrvesh wrote:

i just installed cube ide and initialized ports for my H653ZI board and created IOC file but not able to build projects in it getting these errors


After creating the IOC file, you also need to generate code - did you do that?

As @tjaekel said, this doesn't seem to have anything to do with your title, "Only half of the pins are getting declared in CubeIDE"