[Need Help] Hard Fault Analysis On LR after ADC check HAL_OK
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-02 8:00 PM - last edited on ‎2024-01-05 4:18 AM by mƎALLEm
-
Use different ADC Channels from ADC1 only (just 1 ADC, multi channel) to read 3 sensors.
-
Each time i about to read any ADC channel i configure the channels (e.g 2 or 5) >> start hadc1 >> poll conversion >> get the value >> stop hadc1 and i repeat that for other channels.
-
After some calculation programs i fetch it to USART
I think the bad LR address might be the problem, i.e. reffering to the non-exist address in disassembly, note that in disassembly window (number 2) there is no address 0x8000955 after 0x08000954, but it goes straight to 0x8000956 instead.
- Labels:
-
ADC
-
Flash
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-03 12:54 AM
Hello @dios_kuri,
Could you please share your project?
Thank you!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-03 2:14 AM - edited ‎2024-01-03 2:22 AM
>The LR (call return address) has the adress 0x08000955 whis is not listed in the dissasembly
The address is actually 0x08000954. (Clear the lowest bit. this is because of thumb instruction set TL;DR)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-03 6:46 AM
Thanks for the insight, Pavel. But I am sorry i don't understand how to clear the lowest bit, and i dont know where to put it since the code is an if code to check if hal_adc_configchannel is OK. May i get an example?
Any kind of suggestion helps.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-03 6:53 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-03 7:01 AM
Inconveniently you truncate the register display in the screen shot.
Problem is likely with one of the parameters / structures passed to HAL_ADC_ConfigChannel()
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-03 7:04 AM
More registers, denser display
https://github.com/cturvey/RandomNinjaChef/blob/main/KeilHardFault.c
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-03 7:21 AM
Hi Tesla.
Below the complete view of the registers, printf debug, and disassembly window. Hope this can give more insight. The code is slightly different then the one i posted, but the problem is still the same (i.e. LR address doesnt exist and on the same line of code which is for checking if hal config adc is OK.
Many thanks in advance.
-Dios
==================================================
Line of code
==================================================
Registers:
==================================================
full printf debug window:
==================================================
Disassembly window:
 
==================================================
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-03 8:35 AM
> LR address doesnt exist
As @Pavel A. said, [in your head] mask the LR LSB (set it to 0) to get 0x8001ec2 AS THE RETURN ADDRESS.
But LR is not what you should be paying attention to. Look at the PC value 0x8000203a, THAT is where the problem was. As @Tesla DeLorean said, it is probably an issue with the configuration structure you pass (0 in some field that expects a non-zero value, perhaps).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-03 9:01 AM
You're interested in the code that faults, not the return address for the last function call.
The fault is likely somewhere in HAL_ADC_ConfigChannel() when you use the parameters / pointers passed in. Probably &hadc1
Suggest if you have printf() working, that a) you print out the pointer "%p", b) dump out the structure, and c) the pointer for hadc->Instance
Up vote any posts that you find helpful, it shows what's working..