cancel
Showing results for 
Search instead for 
Did you mean: 

Need advices for STM32F7 bootloader (SD or USB)

rBlr
Associate III

Hello

I`d like to make bootloader for STM32F7 MCU and have few question how to starting with it.

I found `AN4854-IAP_OVER_SDIO` example but can't figure out how to proper open it in ST CubeIDE, which folder or file should be selected as root.

And another question if it is possible to update MCU firmware (user program) via USB flash drive (not SD card) when device should be updated by end user.

Thank you.

0 REPLIES 0