2023-11-15 09:13 PM
While powering up all of my Microcontrollers were getting shorted, checked the voltages of all the capacitors and the MCU has a dedicated power line . And checked the ripple and initial power up data,everything is fine only. But still the MCU getting shorted. Is it because of the batch of the purticular MCU (
STM32F405ZGT6W
2023-11-16 12:50 AM
Welcome @Bosss, to the community!
First of all, I would like to ask you to use a higher resolution when uploading the images so that you can still read something.
By the way, what do you mean by "getting shorted"? If it is original devices from ST and not fakes, I can assure you that all STM32s are fully tested and functional.
What type is used for Y1 (practically unreadable)?
BTW - what is the reason for
Regards
/Peter
2023-11-16 03:26 AM
And that diode at pin PA9 (?) looks suspicious, if PA9 is configured as output with 0V.
And have you double-checked all the VCC / GND pins?
2023-11-16 06:03 AM
Y1: ECS-120-8-33-JGN-TR3
D31(RBS2MM40BTR)- Diode on the JTAG pin is for unidirectional action
2023-11-16 06:05 AM
And that diode at pin PA9 ? (SS2P3-M3/84A)- It is to show that it is a unidirectional action
And have you double-checked all the VCC / GND pins? Yes double checked everything is fine only
2023-11-16 06:46 AM
It certainly has nothing to do with your problem, but it is not necessary to provide NRST with a pull-up because there is one internally in the STM32 (see RM0090, section 6.1.2).
But it would be important to know what you mean by "getting shorted"?
2023-11-23 09:13 PM
No, none of the answers resolved my issue
2023-11-24 06:49 AM
Maybe you could actually answer Peter's question regarding what you mean by "getting shorted".