2023-05-16 6:51 PM - edited 2023-11-20 5:19 AM
I am trying to us the LPTIM low power timer to trigger interrupts intermittently while the MCU is in STOP2 mode, but I am unable to do so. I am testing the interrupts by toggling a GPIO pin and checking the output on a scope.
Without STOP mode I see the interrupts and GPIO toggle as expected. Once I enter STOP2 mode I don't see any interrupts. Interestingly, if I debug the microcontroller via STLINK, I can see the GPIO toggle and a single interrupt trigger if I pause and then resume the debugger.
Is the LPTIM capable of doing this? I want to achieve repeated wake events to perform actions at specified times. The datasheet and reference manual say the LPTIM1 should be fully functional in this low power mode. If this is possible, what am I missing?
Using STMcube to configure the LPTIM and enable interrupts. I have tried configuring with LSI, MSI, and LSE as clock sources.
I am using HAL_LPTIM_Counter_Start_IT(&hlptim1) to start the interrupts and have used callbacks: LPTIM1_IRQHandler() and HAL_LPTIM_AutoReloadMatchCallback().
I am using the development kit B-U585I-IOT02A Discovery.
Some excerpts from the code:
/**
* Enter stop 2 mode
*/
void GoToSleep()
{
__disable_irq(); //Disable interrupt to avoid timing issues
HAL_SuspendTick();
// Useful if already in low power run mode, see https://community.st.com/s/question/0D50X00009XkWAMSA3/stop2-mode-voltage-regulator-stm32cube
// HAL_PWREx_DisableLowPowerRunMode();
is_asleep = true;
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
HAL_ResumeTick();
__enable_irq();
}
/**
* Interrupt that results in wake from stop 2 mode
*/
void HAL_LPTIM_AutoReloadMatchCallback(LPTIM_HandleTypeDef *hlptim)
{
interrupts++;
if(hlptim == &hlptim1)
{
toggle = true;
}
}
/* In main: */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
__HAL_RCC_LPTIM1_CLK_SLEEP_ENABLE();
HAL_StatusTypeDef status = HAL_LPTIM_Counter_Start_IT(&hlptim1);
(void)status;
while (1)
{
if(toggle == true)
{
if(is_asleep == true)
{
SystemClock_Config(); // Need to reconfigure the clock on exit from sleep mode to use HSI clock
is_asleep = false;
}
HAL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin);
toggle = false;
}
GoToSleep();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
2023-05-16 11:22 PM
Did you try it without debug mode?
2023-05-17 5:24 AM
Yes. I have tried deploying through debug mode and then disconnecting the debugger and restarting the MCU.
Also tried compiling in Release configuration and flashing the MCU manually.
Neither works
2023-05-17 7:20 AM
I tried the same code with a similar configuration on a different development kit, the STM32L562E-DK Discovery. It works as expected there. Still not working on the STM32u585
2023-05-17 9:16 AM
Managed to solve this thanks to https://community.st.com/s/question/0D53W00001zhW8ISAU/port-application-from-stm32l4-to-stm32u5-waking-from-stop2-by-lpuart-rtc-etc.
Needed to set the LPTIM1AMEN bit in the RCC_SRDAMR register to enable autonomous mode in stop mode.
Used the __HAL_RCC_LPTIM1_CLKAM_ENABLE(); macro to do this.
2023-05-19 8:44 AM
Hello @JKahn.1,
Glad that you managed to solve your problem, by using STM32U5 you can use the LPBAM feature that allows LPTIM to request its clock and can stay functional in stop2 mod without even waking up the CPU!
Check this knowledge article about the feature and its advantages
I hope that helps in your future projects!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.