Skip to main content
mh_stm
Associate II
Jun 28, 2018 11:29 AM UTC
Question

STOP2 mode, voltage regulator, stm32cube

Posted on June 28, 2018 at 13:29

Hi all,

I'm trying low power modes of the STM32. I've noticed that HAL_PWREx_EnterSTOP2Mode synopsis mention that:

  *        The voltage regulator is set in low-power mode but LPR bit must be cleared to enter stop 2 mode.

  *        Otherwise, Stop 1 mode is entered.  

however

/STM32Cube_FW_L4_V1.11.0/Projects/NUCLEO-L476RG/Examples/PWR/PWR_STOP2_RTC/Src/

does not include such thing. and AN4621 indicates that LowPowerRun mode doesn't get involved when switching between Run mode and Stop2 modes.

Therefore I see contradiction.  Could any one clarify please ?

Thanks,

    This topic has been closed for replies.

    2 replies

    Szymon PANECKI
    Senior III
    Jun 28, 2018 12:47 PM UTC
    Posted on June 28, 2018 at 14:47

    Hello Mohamed,

    LPR is a name of a bit in PWR_CR1 register. You can find its description in MCU's reference manual. I attach extracted content below:

    0690X0000060LVHQA2.png

    As you can see this bit allows MCU to enter Low-power RUN mode. There is also confirmation that this bit needs to be cleared before entering STOP mode in order to achieve STOP2 instead of STOP1.

    The outcome of this description is a message, that STM32L4 MCU can't make a switch from Low-power RUN to STOP2 directly. If application uses Low-power RUN, then it is mandatory to make a switch from Low-power RUN to RUN and then from RUN to STOP2. Please find below a simple diagram, which shows possible transistions in terms of operating modes.

    0690X0000060LVRQA2.png

    Now regarding the code: this is correct that HAL_PWREx_EnterSTOP2Mode function doesn't clear LPR bit. So this action has to be done by other function, which is HAL_PWREx_DisableLowPowerRunMode. But please note: this function needs to be called before HAL_PWREx_EnterSTOP2Mode

    only

    when MCU is using low-power RUN mode. Otherwise, if normal RUN mode is used, LPR bit is set to 0 and there is no need to take care about this bit.

    I hope this information properly answers your question.

    Regards

    Szymon
    mh_stm
    mh_stmAuthor
    Associate II
    Feb 27, 2019 10:52 AM UTC

    Hello Szymon,

    Thank you for you support. This is a useful information.

    Regards,